Skip to main content
PVZ
Associate II
May 20, 2020
Question

Problem with HRTIM with Nucleo-H743ZI2 Board

  • May 20, 2020
  • 6 replies
  • 2234 views

Hello Everybody

I have the Problem with my Hightimer PWM Output.

If I define that my HRTIM is working with 480MHz (CPU_Ck).

it will not and work with the normal 240MHz Output.

Why is that so?

This topic has been closed for replies.

6 replies

TDK
May 20, 2020

Are you trying to get a PWM signal at 240MHz? That's above the max frequency of the GPIO pins.

"If you feel a post has answered your question, please click ""Accept as Solution""."
PVZ
PVZAuthor
Associate II
May 20, 2020

Thanks for the answer

No sorry i have made a mistake while i was uploading the pictures

I try to get a faster 10 Bit PWM signal, because of that i need the high resolution timer with 480MHz instead of 240MHz.

PVZ
PVZAuthor
Associate II
May 20, 2020

..

PVZ
PVZAuthor
Associate II
May 20, 2020

0693W000001ccE1QAI.png

PVZ
PVZAuthor
Associate II
May 20, 2020

0693W000001ccEBQAY.png

PVZ
PVZAuthor
Associate II
May 20, 2020

0693W000001ccbKQAQ.jpg