Steval-SPIN3202 Hoverboard Hall Sensors bring Speed Feedback Error when Starting
Hello,
I'm new to STM32 programming but now I have already tried a lot and read quite a bit.
I have a Steval Spin3202 and Spin3201 board (just tested the 3202 yet) and i want to drive two unknown Hoverboard motors with the boards.
I have created a ST Motor Control Workbench projekt and selected the board.
I added the motor parameter and set the Hallsensor to 60° but already tried 120° as well.
Now i have the set the speed Sensing to Hall with 6 fault measurements before Error.
The Voltage Jumper is set to 3.3V and I see that the Voltage drops/rises when spinning the wheel while observing with the voltmeter.
When I start the motor i just see a very small "jump" and then the feedback occures.
I was hoping to have a better drive experience then with Sensorless measurement (that already kind of worked with a ramp and some adjustment, but not very well when Load was applied).
The motor has hall-sensors installed, but i also don't know the characteristics.
My motor should look like this -->