Associate III
May 18, 2020
Question
FSMC with NAND interface signalling
- May 18, 2020
- 2 replies
- 2907 views
Hello, I am using STM32L4R9AI (attached the reference manual) with 128GB NAND flash (MT29F128G08CFABBWP-12IT:B TR) (attached its datasheet).
1- This is 8bit NAND flash and according to page 104 in the reference manual the last signal is NWAIT/INT which goes to R/B# according to page 9 in the NAND datasheet, should I connect R/B# from memory to FMC_NWAIT (PD6) or FMC_INT (PG7) ?
2- what are common/attrtibute space timing (in HCLK cycles) for (setup, wait, hold, hi-z) ?
Thanks in advance.