Skip to main content
spark.1
Visitor II
May 13, 2020
Question

Not getting interrupt of Timer2 input capture in STM8S003F3 .

  • May 13, 2020
  • 0 replies
  • 856 views

Hi,

I am using input capture of Timer2 Ch1 in stm8s003f3(20 pin uC). I had configured the timer 2 and provided pulses in PD4 pin , but i am not getting interrupt in Timer2 interrupt handler.

void InitTimer2(void)

{

TIM2_DeInit();

CLK->PCKENR1 |= 0x20;      //Enable Peripheral Clock Tim1

//GPIOD->DDR &= 0xF7;

//GPIOD->CR1 |= 0x08;

TIM2->IER |= 0x02; //0x02      //Capture1 interrupt enable

//TIM2->EGR |= 0x02;

TIM2->CCMR1 |= 0x01; // CC1 channel is configured as input

TIM2->CCER1 |= 0x01; //Enable capture

TIM2->PSCR |= 0x07;       //16MHZ/128 = 125KHZ

TIM2->ARRH = 0;

TIM2->ARRL = 0xFF; //8us counter

TIM2->CR1 = 0x01;

}

INTERRUPT_HANDLER(TIM2_CAP_COM_IRQHandler, 14)

{

 /* In order to detect unexpected events during development,

 it is recommended to set a breakpoint on the following instruction.

 */

TIM2->SR1 = 0;

Count0= TIM2->CCR1L;

if (Count0 > Count1) 

{

Count = (unsigned int)(Count0 - Count1);

}

else if (Count0 < Count1) 

{

//Count = (unsigned int)(Count0 + (0xFFFFFFFF - Count1) + 1);

var1 = (0xFF - Count1);

var1 += 1;

Count = (unsigned int)(Count0 + var1);

}

else if (Count0 == Count1) 

{

Count = (unsigned int)(0);  

}

Count1 = Count0;

}

what is the mistake i have done ?. Plz anyone support very urgent.

    This topic has been closed for replies.