Question
Added Custom Board from CubeMx, but an error occour
Hi St-Community,
im hanging around with the following Problem:
I build up a yocto environment and build sucessfully images. No its time to add a custom devicetree to the linux.
So i followed the instructions on:
https://wiki.st.com/stm32mpu/wiki/How_to_create_your_own_machine
But i get the following error when i start to build a image with bitbake image-base-minimal.
ERROR: u-boot-stm32mp-extlinux-2.0-r0 do_create_multiextlinux_config: No UBOOT_EXTLINUX_CONFIG_FLAGS list defined, nothing to do
ERROR: u-boot-stm32mp-extlinux-2.0-r0 do_create_multiextlinux_config: Function failed: update_extlinuxconf_targets
ERROR: Logfile of failure stored in: /opt/build/tmp/work/stm32mp1_mustera-poky-linux-gnueabi/u-boot-stm32mp-extlinux/2.0-r0/temp/log.do_create_multiextlinux_config.5058
ERROR: Task (/opt/yocto/meta-st-stm32mp/recipes-bsp/u-boot/u-boot-stm32mp-extlinux.bb:do_create_multiextlinux_config) failed with exit code '1'Have you any hints to me where i can debug. I dont know wehere these variables are defined.
Best regards and many thanks
Niklas