Skip to main content
vegetableswim
Visitor II
May 4, 2020
Question

STM8L051 ADC Pin current consumption when HALT

  • May 4, 2020
  • 1 reply
  • 1022 views

Using STM8L051 ADC PD0, 3.7V~4.2V Li-Po battery, 1M+1M resistor to divde the battery voltage, 100nF capacitor to GND.

If set PD0 floating input and halt, total current 40uA, if set PD0 push-pull output LOW, 10uA. But the drawback of output LOW is that I have to wait 350ms for the 100nF cap charging before a new ADC reading.

Is there any method to reduce current consumption and remain floating input?

 GPIOD->CR2 &= ~0x01; // External interrupt disable
 GPIOD->CR1 &= ~0x01; // Floating input
 GPIOD->DDR &= ~0x01; // Input
 delay_ms(350); //Waiting capacitor charging and stable
 
 /* Enable ADC1 peripheral clock*/
 CLK->PCKENR2 |= 1<<0;
 /*clear CR1 register */
 ADC1->CR1 = 0x00;
 /* set the resolution and the conversion mode */
 ADC1->CR1 |= 1<<2; //continuous mode, 12bit
 //ADC1->CR1 &= ~(1<<2); //single mode, 12bit
 /*clear CR2 register */
 ADC1->CR2 &= ~0x80;
 /* set the Prescaler */
 ADC1->CR2 |= 0x80; //CLK/2
 /* Configures the sampling time for the Slow ADC channel group. */
 ADC1->CR2 &= ~0x07;
 ADC1->CR2 |= 0x07; //384 cycles
 /* Set the ADON bit to wake up the specified ADC from power down mode */
 ADC1->CR1 |= 0x01;
 /* Enable the selected ADC channel(s). */
 ADC1->SQR[1] |= 1<<6; //SQR2, PD0 channel 22
 /* Clear EOC flag */
 //ADC1->SR &= ~0x01;
 /* Start the ADC software conversion */
 ADC1->CR1 |= 0x02;
 
 
 for(i=0;i<8;i++)
 {
 //ADC1->CR1 |= 0x02;
 while((ADC1->SR & 0x01) == 0x00);
 temp = (uint16_t)(ADC1->DRH);
 temp = (uint16_t)((uint16_t)((uint16_t)temp << 8) | ADC1->DRL);
 ADCdata += temp;
 }
 ADCdata >>= 3;
 
 
 /* power down mode */
 ADC1->CR1 &= ~0x01;
 /* Disable the selected ADC channel(s). */
 ADC1->SQR[1] &= ~(1<<6); //SQR2, PD0 channel 22
 /* Disable ADC1 peripheral clock*/
 CLK->PCKENR2 &= ~0x01;
 
 // PD0, ADC_IN
 GPIOD->CR2 &= ~0x01; // 2MHz slow
 GPIOD->CR1 |= 0x01; // Push-pull
 GPIOD->ODR &= ~0x01; // Output Low
 GPIOD->DDR |= 0x01; // Output

    This topic has been closed for replies.

    1 reply

    RusikOk
    Associate III
    August 15, 2020

    to control the supply voltage, you can use the following approach https://electronix.ru/forum/index.php?app=forums&module=forums&controller=topic&id=128726