2020-05-03 5:58 AM
When I want to use the X-CUBE-BLE1.5.0.0 on STM32CubeMX, the file "b_l475e_iot01a1_bus.h/c" is not generated. Thus the project cannot be compiled.
To reproduce:
See attached file...
2020-05-07 5:33 AM
Hi,
thanks for reporting this issue. It will be fixed.
As workaround, I can suggest you to:
Please, see the attached .ioc file.
BR
Silvio
2020-05-07 7:45 AM
Hello,
that workaround does not work for me, I also tried the ioc you attached.
2020-05-07 9:05 AM
Hello,
what type of error you are facing?
What version of STM32CubeMX are you using?
Did you try to create your project from scratch?
BR
Silvio
2020-05-07 11:32 PM
Hi Silvio,
I use Cube IDE ( from "About" page):
STM32CubeIDE Version: 1.3.1 Build: 6291_20200406_0752 (UTC)
STM32CubeMX 5.6.1.202004052303 com.st.stm32cube.common.feature.mx
I created the project from scratch as follows:
If i select X-CUBE-BL1 components, for version 5.0.0, it displays errors for Controller and HCI_TL saying, the components have unresolved dependencies, and no solution found. See attached picture.
If I select 4.4.0, it says this version is not compatible with the current version of cube mx. see attached pic.
No other version option is listed.
I configure the pins as in the first post.
When I want to build, I get the follwoing with both configs:
If I clear the pins as you suggested, it is all the same.
If I use your attached ioc, it is all the same.
I cannot change the app structure at code generation, it is disabled:
compile output:
arm-none-eabi-gcc "../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32L475xx -c -I../Middlewares/ST/Middlewares/ST/BlueNRG-MS/includes -I../Middlewares/ST/Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Template -I../BlueNRG-MS/Target -I../Middlewares/ST/BlueNRG-MS/utils -I../Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Basic -I../Middlewares/ST/BlueNRG-MS/includes -I../Drivers/CMSIS/Include -I../Core/Inc -I../Drivers/BSP/CUSTOM -I../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../Drivers/STM32L4xx_HAL_Driver/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.d" -MT"Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.o"
../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_IFR.c:356:2: warning: #warning BLUENRG_CONFIG not valid [-Wcpp]
#warning BLUENRG_CONFIG not valid
^~~~~~~
In file included from ../Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Basic/hci_tl.h:19:0,
from ../Middlewares/ST/BlueNRG-MS/includes/hci_const.h:14,
from ../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_gap_aci.c:18:
../BlueNRG-MS/Target/hci_tl_interface.h:33:10: fatal error: b_l475e_iot01a1_bus.h: No such file or directory
#include "b_l475e_iot01a1_bus.h"arm-none-eabi-gcc "../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DDEBUG -DSTM32L475xx -c -I../Middlewares/ST/Middlewares/ST/BlueNRG-MS/includes -I../Middlewares/ST/Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Template -I../BlueNRG-MS/Target -I../Middlewares/ST/BlueNRG-MS/utils -I../Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Basic -I../Middlewares/ST/BlueNRG-MS/includes -I../Drivers/CMSIS/Include -I../Core/Inc -I../Drivers/BSP/CUSTOM -I../Drivers/CMSIS/Device/ST/STM32L4xx/Include -I../Drivers/STM32L4xx_HAL_Driver/Inc -I../Drivers/STM32L4xx_HAL_Driver/Inc/Legacy -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.d" -MT"Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_updater_aci.o"
../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_IFR.c:356:2: warning: #warning BLUENRG_CONFIG not valid [-Wcpp]
#warning BLUENRG_CONFIG not valid
^~~~~~~
In file included from ../Middlewares/ST/BlueNRG-MS/hci/hci_tl_patterns/Basic/hci_tl.h:19:0,
from ../Middlewares/ST/BlueNRG-MS/includes/hci_const.h:14,
from ../Middlewares/ST/BlueNRG-MS/hci/controller/bluenrg_gap_aci.c:18:
../BlueNRG-MS/Target/hci_tl_interface.h:33:10: fatal error: b_l475e_iot01a1_bus.h: No such file or directory
#include "b_l475e_iot01a1_bus.h"As far as I can recall, it worked well with x-cube-ble1 4.2.x
2020-05-08 12:38 AM
Hi blacix,
you could directly use the latest STM32CubeMX v5.6.1 to configure the B-L475E-IOT01A1 and generate a project for the STM32CubeIDE.
BR
Silvio
2020-05-08 12:43 AM
OK, thanks, I'll give it a shot.
2020-05-08 1:05 AM
Hi,
you can for sure continue using STM32CubeIDE for your projects.
Clearly, the issue you faced will be fixed.
Thanks!
BR
Silvio
2020-05-08 1:17 AM
If I use the standalone mx ( which is the same version as the one in IDE though ) It works, well, almost...
The generated b_l475e_iot01a1_bus.c cannot be compiled, because it cannot find the configured pins, which are defined in main.h
Inlcuding main.h in that file solves the issue, but it is still very annoying, since a generated file needs to be modified after any change made to the mx project.
I guess, that's the reason for your suggestion of clearing the pins.
I hope this is going to be resolved soon because I will have to work a lot with this board...
Thanks for your help, and thanks in advance!
2020-05-09 9:32 AM
Hi Silvio, blacix,
the problem of the not found "configured pins, which are defined in main.h" seems to be the same problem (or similar) as the one I reported in "BUG report on code generation STM32L476":
May be this idea can help to find the solution...