Associate III
May 2, 2020
Question
Text wildCard shows characters
- May 2, 2020
- 5 replies
- 1261 views
Hello,
I made a simple project to test TouchGFX, when I move the slider I got error values, the initial value I’ve set in TouchGFX Designer is 25, so when I move the slider if the value contains 2 or 5 it will show with an other character
this is is my code:
void Screen1View::SliderChanged(int value)
{
unicode::snprintf(textArea1Buffer, TEXTAREA1_SIZE, “%d�?,value );
textArea1.setWildcard(textArea1Buffer);
textArea1.invalidate();
}