Skip to main content
GStew
Visitor II
April 29, 2020
Question

When I increase the spreading factor on my CMWX1ZZABZ, which uses a STM32L and SX1276, I keep getting a OnTxTimeout.

  • April 29, 2020
  • 1 reply
  • 635 views

If the spreading factor is set to 9, messages get through. As I increase it to 10 or 11, I start to get the OnTxTimeout error. The payload I'm sending is similar to this

lCrTHfXrQdM7M6ZoFrmwMxHacVtZcoBxvSvve0Pi5awSYtk=

I need to increase the spreading factor to increase the range. My frequency is set to 904600000 and my bandwidth is set to 2.

This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
April 29, 2020

You'll need to expand the timeout to accommodate the amount of time it takes to send the message.

Perhaps use Semtech's LoRa Calculator to understand the timing/constraints.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..