Skip to main content
Jblan.1
Visitor II
April 28, 2020
Question

Can I connect this device on a charge without other components ? Can I upload some algorithm on the MCU ? Can I connect the EVAL-L9963-NDS with this device for two battery pack in parallel ?

  • April 28, 2020
  • 1 reply
  • 661 views

Dear Madam and Mister,

I am an french intern engineer, and I search a battery monitor. I would like used the EVAL-L9963-MCU to upload some algorithm about the state of the battery and connect this device on a test bench. So, I have some question :

Can I connect this device on a charge without other components ?

Can I upload some algorithm on the MCU ?

Can I connect the EVAL-L9963-NDS with this device for two battery pack in parallel ?

Thank you in advance for your attention.

Sincerely,

Jérémy

This topic has been closed for replies.

1 reply

PSavv.1
Associate
March 31, 2021

I have the same 2nd question does this thread is solved? I also want to know if there is a Schematic Cad file for the EVAL-L9963-MCU.

Thanks in advance.