Skip to main content
AShva.1
Associate III
April 22, 2020
Question

Openbox-session not started :(

  • April 22, 2020
  • 2 replies
  • 1066 views

Hi!

I installed st-example-image-x11 on the board STM32MP157x-DK2.

I can not log in :(

In the comments, I read that I need to fix the rootfs / etc / lxdm / lxdm.conf file.

Here is the file with my corrections

[base]

## uncomment and set autologin username to enable autologin

autologin=root

## uncomment and set timeout to enable timeout autologin,

## the value should >=5

#timeout=10

## default session or desktop used when no systemwide config

#session=/usr/bin/startlxde

session=/usr/bin/openbox-session

## uncomment and set to set numlock on your keyboard

# numlock=0

## set this if you don't want to put xauth file at ~/.Xauthority

# xauth_path=/tmp

# not ask password for users who have empty password

skip_password=1

## greeter used to welcome the user

greeter=/usr/libexec/lxdm-greeter-gtk

[server]

## arg used to start xserver, not fully function

arg=/usr/bin/X -s 0

# uncomment this if you really want xserver listen to tcp

# tcp_listen=1

# uncoment this if you want reset the xserver after logou

# reset=1

[display]

## gtk theme used by greeter

gtk_theme=Clearlooks

## background of the greeter

# bg=/usr/share/backgrounds/default.png

## if show bottom pane

bottom_pane=1

## if show language select control

lang=1

## if show keyboard layout select control

keyboard=0

## the theme of greeter

theme=Industrial

[input]

[userlist]

## if disable the user list control at greeter

disable=0

## whitelist user

white=root

## blacklist user

black=

I think the window manager name is incorrect (highlighted in black)

I did not find a file named openbox-session in the /usr/bin/ directory.

What you need to do to log in to the system?

Best regard

Alexander

This topic has been closed for replies.

2 replies

mleo
Visitor II
April 28, 2020

Hi Alexander,

The issue was reproduces and exoerts asked for help.

I'll come back to you when reaply is available.

Milan

AShva.1
AShva.1Author
Associate III
April 28, 2020

Hi Milan!

I solved this problem. :)

The image st-example-image-x11 uses the MATCHBOX window manager.

The line should be like this:

session=/usr/bin/matchbox-session

Best regard

Alexander

P.S.

A new problem has appeared: can't change matchbox-panel orientation :(