Skip to main content
JBeca.1
Associate II
April 21, 2020
Question

RTOS (freertos) debug support over STM32CubeIDE

  • April 21, 2020
  • 9 replies
  • 2929 views

Dear all,

I'm trying to debug FreeRTOS over STM32F7/F3/F4 but I don't get it.

With STLINK gdb server debugger, i can debug but only see 1 task in debugger panel.

I tried with openOCD but it not works...

Anyone do it before?

Thanks

Regards

This topic has been closed for replies.

9 replies

Panometric
Associate III
April 21, 2020

You need to add a user defined configuration script:

Here's an example. The key is the last line: "$_TARGETNAME configure -rtos FreeRTOS"

# This is an genericBoard board with a single STM32L476RGTx chip
#
# Generated by STM32CubeIDE
# Take care that such file, as generated, may be overridden without any early notice. Please have a look to debug launch configuration setup(s)
 
source [find interface/stlink.cfg]
 
set WORKAREASIZE 0x8000
 
transport select "hla_swd"
 
set CHIPNAME STM32L476JEYX
 
# Enable debug when in low power modes
set ENABLE_LOW_POWER 1
 
# Stop Watchdog counters when halt
set STOP_WATCHDOG 1
 
# STlink Debug clock frequency
set CLOCK_FREQ 8000
 
# Reset configuration
# use hardware reset, connect under reset
# connect_assert_srst needed if low power mode application running (WFI...)
reset_config srst_only srst_nogate connect_assert_srst
set CONNECT_UNDER_RESET 1
set CORE_RESET 0
 
# BCTM CPU variables
 
source [find target/stm32l4x.cfg]
$_TARGETNAME configure -rtos FreeRTOS

JBeca.1
JBeca.1Author
Associate II
April 22, 2020

Hi,

thanks for the feedback.

I tried it before, and it not works...

This is my ouptut with OCD debugger

Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:54)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 8000 kHz
Info : STLINK V2J36S26 (API v2) VID:PID 0483:374B
Info : using stlink api v2
Info : Target voltage: 3.235194
Info : SRST line asserted
Warn : Silicon bug: single stepping will enter pending exception handler!
Info : STM32F746ZGTx.cpu: hardware has 8 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Error: No symbols for FreeRTOS
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08003828 msp: 0x20050000
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
adapter speed: 4000 kHz
Info : device id = 0x10016449
Info : flash size = 1024kbytes
Info : SRST line asserted
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08003828 msp: 0x20050000
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
adapter speed: 4000 kHz
Info : Padding image section 0 at 0x080001c8 with 8 bytes
target halted due to breakpoint, current mode: Thread 
xPSR: 0x61000000 pc: 0x20000044 msp: 0x20050000
Info : SRST line asserted
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08003828 msp: 0x20050000
Error: Error: null stack pointer in thread
Error: RTOS: failed to get register list
Error: Error: null stack pointer in thread
Error: RTOS: failed to get register list
Error: Error: null stack pointer in thread
Error: RTOS: failed to get register list

Pavel A.
April 25, 2020

Does "ST-LINK GDB server" have an option similar to $_TARGETNAME configure -rtos FreeRTOS ?

Or must use OpenOCD to have RTOS support?

-- pa

Panometric
Associate III
April 25, 2020

Not that I'm aware. I think OpenOCD is the only way to get thread aware debugging in STM32 with STLINK anyway.

JBeca.1
JBeca.1Author
Associate II
April 27, 2020

Hi,

correct, only OpenOCD has multitask debug support.

ST-LINK GDB is an option to debug, but you only see 1 task.

@Panometric​ any idea about OpenOCD not works in my case?

Thanks

Regards

Jordi

Panometric
Associate III
May 18, 2020

@JBeca.1 I don't see that error. It suggests your RTOS is not linked in. I did notice this other part that I had applied though.

Put this in a .C file:

#include "FreeRTOS.h"
 
#ifdef __GNUC__
#define USED __attribute__((used))
#else
#define USED
#endif
 
const int USED uxTopUsedPriority = configMAX_PRIORITIES - 1;

 And put this in the linker settings:

-Wl,--undefined=uxTopUsedPriority

And here's the guide I used to figure it out.

https://mcuoneclipse.com/2016/04/09/freertos-thread-debugging-with-eclipse-and-openocd/

JBeca.1
JBeca.1Author
Associate II
May 28, 2020

HI @Panometric​ ,

thanks for your support. I tried it... but it doesn't work.

I added the code in main.c

And the linker setting I added in build options (see image)

0693W000001pb2oQAA.png

I can "enter in debug mode" but debugger not works. The eclipse show that app is running, but I can't resume, stop, step, ... and board doesn't do a nything

I attach the console output

Thanks for your tiem

Regards

Jordi

Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:54)
Licensed under GNU GPL v2
For bug reports, read
	http://openocd.org/doc/doxygen/bugs.html
srst_only separate srst_nogate srst_open_drain connect_assert_srst
Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD
adapter speed: 8000 kHz
adapter_nsrst_delay: 100
Info : Listening on port 6666 for tcl connections
Info : Listening on port 4444 for telnet connections
Info : clock speed 8000 kHz
Info : STLINK V2J36S26 (API v2) VID:PID 0483:374B
Info : using stlink api v2
Info : Target voltage: 3.244649
Info : SRST line asserted
Info : STM32F334R8Tx.cpu: hardware has 6 breakpoints, 4 watchpoints
Info : Listening on port 3333 for gdb connections
Info : accepting 'gdb' connection on tcp/3333
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08000640 msp: 0x20003000
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
adapter speed: 4000 kHz
Info : device id = 0x10016438
Info : flash size = 64kbytes
Info : Auto-detected RTOS: FreeRTOS
Info : SRST line asserted
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08000640 msp: 0x20003000
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
Info : Unable to match requested speed 8000 kHz, using 4000 kHz
adapter speed: 4000 kHz
Info : Padding image section 0 at 0x08000188 with 8 bytes
target halted due to breakpoint, current mode: Thread 
xPSR: 0x61000000 pc: 0x2000003a msp: 0x20003000
Info : SRST line asserted
Info : SRST line released
target halted due to debug-request, current mode: Thread 
xPSR: 0x01000000 pc: 0x08000640 msp: 0x20003000
Error: Error reading stack frame from thread
Error: RTOS: failed to get register list
Error: Error reading stack frame from thread
Error: RTOS: failed to get register list

JBeca.1
JBeca.1Author
Associate II
September 4, 2020

@KOkun.1048​ 

Hi,

sorry for the delay in my answer.

I check your link, but it not works....

I will answer in the other thread.

Thanks

Jordi