Skip to main content
David Martins
Senior
April 21, 2020
Question

How to tune Torque (current) Control?

  • April 21, 2020
  • 7 replies
  • 2446 views

Hello everyone!

Well, the question is this: what is the procedure for tuning the Torque/Current Controller?

About the Speed Controller, it is well known how to tune the gains of the PID. In addition to the ST documentation - AN5464 - it is possible to see an explanation of the empirical method.

However, I don't find in the documentation information about the Torque/Current tuning. I can observe the Iq through the DAC, but the rest of the procedure I need help.

Thank you!

This topic has been closed for replies.

7 replies

Laurent Ca...
Senior III
September 11, 2020

Dear David Martins

Do you have still this problem to solve?

Best regards

Laurent Capella

David Martins
Senior
September 11, 2020

The project is in a standby phase.... but yes, the torque tunning problem persist.

KKuma.3
Associate
October 12, 2020

@Laurent Ca...​ Could you please give some hints regarding this question?

Laurent Ca...
Senior III
October 13, 2020

Dear @KKuma.3​ 

Could you give us the details of your materials (HW and SW, boards and tools, ad so on)?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
October 20, 2020

Dear @KKuma.3​ 

Any news?

Best regards

Laurent Ca...

KKuma.3
Associate
October 21, 2020

Hello ,

@Laurent Ca...​ " @STM32 Motor Control " thank you for the reply.

I am using Nucleo F303 RE and X-Nucleo - IHM08M1, MCSDK 5.4.4.

Maxon 70 Watt motor with encoder.

I am able to control the position of the motor with the provided application for a limited speed.

Below are my questions,

1 how can I tune the motor for a better torque performance , for position control application?

2 I wanted to spin the motor at very low speeds, i.e position control at low speeds and higher torque.

The PID tuning explained in AN5464 is not sufficient and does not work.

3 I also wanted to know the impact of using the MCI_SetCurrentReferences api instead of MCI_ExecSpeedRamp or MCI_ExecTorqueRamp ?

4 How do I select the values of current if I use MCI_SetCurrentReferences api in MCboot for a particular motor ?

Regards,

Kumar

CKlei.1
Associate II
November 17, 2021

I'm on the same phase in my project where I need to tune the torque/current controller. I also need to limit the max. current (kind of protection for my power supply). Therefore, it would be very helpful to get some information about the question David Marin has posed.

Regards

Chris Kleiber