Skip to main content
kj.obara
Associate III
April 20, 2020
Question

PDSC schema issues when downloading CMSIS 5.7.0 in STM32CubeMX 5.6.1

  • April 20, 2020
  • 6 replies
  • 1767 views

 Hi,

I've recently started using STM32CubeMX and I tried installing newest Arm CMSIS 5.7.0, but whenever I do that I get the following error.

 Errors: 
 
 - Ërror: Line= 633 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 633 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'processor' is not valid with respect to its type, 'DcoreEnum'.
 - Ërror: Line= 1037 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
- Ërror: Line= 1037 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'accept' is not valid with respect to its type, 'DcoreEnum'.
 - Ërror: Line= 1185 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
 
 - Ërror: Line= 1185 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'require' is not valid with respect to its type, 'DcoreEnum'.
 
 - Ërror: Line= 1189 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.
 - Ërror: Line= 1189 : cvc-attribute.3: The value 'Cortex-M55' of attribute 'Dcore' on element 'accept' is not valid with respect to its type, 'DcoreEnum'.
- Ërror: Line= 1190 : cvc-enumeration-valid: Value 'Cortex-M55' is not facet-valid with respect to enumeration '[SC000, SC300, Cortex-M0, Cortex-M0+, Cortex-M1, Cortex-M23, Cortex-M3, Cortex-M33, Cortex-M35P, Cortex-M4, Cortex-M7, ARMV8MBL, ARMV8MML, ARMV81MML, Cortex-R4, Cortex-R5, Cortex-R7, Cortex-R8, Cortex-A5, Cortex-A7, Cortex-A8, Cortex-A9, Cortex-A15, Cortex-A17, Cortex-A53, Cortex-A57, Cortex-A72, Cortex-A73, other]'. It must be a value from the enumeration.

Obviously there is a problem since CMSIS schema changed to 1.6.3, whereas Schema 1.6.2 which this gets validated against doesn't contain eg. Cortex-M55. CMSIS 5.6.0 installs fine.

Is there any way that I can change the file that is used for this validation?

This is happening on MacOS 10.15.4 with STMCubeMX 5.6.1. I tried looking for the right file inside the app folder and in my ~/.stmcubemx and ~/.stcufinder but couldn't find the right file.

Thank you in advance.

This topic has been closed for replies.

6 replies

Nesrine.JLASSI
Visitor II
April 20, 2020

Hello @kj.obara​ 

Thanks for the feedback, issue detected.

It will be fixed next STM32CubeMX version.

Best regards,

Nesrine

ARagn.1
Associate II
May 7, 2020

I'm facing the same issue, when will it be fixed? can you please give us an idea?

Thanks,

Andrea

PNM.1
Visitor II
May 1, 2020

I am also getting same error still when i try to install CMSIS with either STM32CubeMX or STM32CubeIDE.

When will be the next version release? Please comment

PNM.1
Visitor II
May 1, 2020

Is there way to work around with this issue?