Skip to main content
KJeps.2
Associate
April 20, 2020
Solved

How to write variable from flow in cube-monitor?

  • April 20, 2020
  • 11 replies
  • 3707 views

I think this page would have the content:

https://wiki.st.com/stm32mcu/wiki/STM32CubeMonitor:How_to_write_a_variable_from_flow

It seems that hashKey value can not be read out somewhere?

{"variablelist":[{"address":"{{flow.current_limit_adr}}","name":"current_limit","type":5,"checked":true,"$$hashKey":"object:604","value":"{{payload}}","validity":true}],"accesspoint":0}

(I know how to use the write panel - but need to set 1 variable with value from flow)

This topic has been closed for replies.
Best answer by stephane.legargeant

Hello

To write data by flow, the following payload must be sent to probe out node ,with the topic “write�? :

{

   "variablelist": [

       {

           "address": "0x20000060",

           "type": 4,

           "value": "xxxx"

       }

   ],

   "accesspoint": 0

}

 The question has been asked in this topic : https://community.st.com/s/question/0D53W000000ayg1SAA/hello-how-is-it-possible-to-change-a-variable-by-pressing-a-buttoni-just-can-change-a-variable-by-using-the-write-panel-butregards

The post explains with details how to write variable from the flow without using the write-panel. It should answer you point.

We are preparing a wiki page, but it is not finalized yet. So there is just a placeholder right now on the wiki.

best regards

Stephane

11 replies

stephane.legargeant
ST Employee
April 20, 2020

Hello

To write data by flow, the following payload must be sent to probe out node ,with the topic “write�? :

{

   "variablelist": [

       {

           "address": "0x20000060",

           "type": 4,

           "value": "xxxx"

       }

   ],

   "accesspoint": 0

}

 The question has been asked in this topic : https://community.st.com/s/question/0D53W000000ayg1SAA/hello-how-is-it-possible-to-change-a-variable-by-pressing-a-buttoni-just-can-change-a-variable-by-using-the-write-panel-butregards

The post explains with details how to write variable from the flow without using the write-panel. It should answer you point.

We are preparing a wiki page, but it is not finalized yet. So there is just a placeholder right now on the wiki.

best regards

Stephane

KJeps.2
KJeps.2Author
Associate
April 20, 2020

Thanks.... I only forgot the "write" topic :(

"$$hashKey":"object:604"

"validity":true

These 2 is for no use?

/Kasper

stephane.legargeant
ST Employee
April 20, 2020

You don't need to take care of "$$hashKey" and "validity" to write from flow.

Stephane

Rghai.1
Associate
November 11, 2021

Hello,

I follow the instruction and i receive this error:

 "Bad parameter (7)"

msg : string[264]

"Unsuccessful write (Bad parameter (7)) on 48FF6E064986484820270787, for data = "{\n \"variablelist\": [\n {\n \"address\": \"0x20000000\",\n \"type\": 3,\n \"value\": \"3678\"\n }\n ],\n \"accesspoint\": 0\n}": write"

Do you know what's wrong with it? I check the address and i type and they are correct.

KJeps.2
KJeps.2Author
Associate
April 20, 2020

Got it - and stuff is working.

This is really a good and powerfull tool you have produced here - Thank you!!

Just as a feedback, i had some problems with adding 2 variables blocks to select different variables, then it uses the same exe config, and mixes up the variables between them.... i ended up using only one variables block and manual parse them out.

On the other hand i could have made several variabel blocks, and connect direct to chart.

/Kasper