Skip to main content
DCiko.1
Associate
April 17, 2020
Solved

Is somehow possible to detect rising and falling edge of input signal ?

  • April 17, 2020
  • 7 replies
  • 6382 views

HI,

I'm using STM32f4 and I'm trying to calculate rotation speed using Hall sensors.

Idea is to use TIM4 and 3 Hall sensors in 3 channels in caputre compare mode to calculate time between two edges. I know how to do that, but the problem is that I need information about the falling or rising edge to know on what angle is rotor.

I need angle to calculate rotation speed, the difference between to captures will never be exactly 60 deegres.

I' am also planing to do calibration of hall sensors to know angle precisely .

So is it possible to detect rising/falling edge using timer or is there some other way to do it ?

Thanks,

Domagoj.

This topic has been closed for replies.
Best answer by DBehe.1

At a time you can either capture rising edge or falling edge but there is a solution initially set the register for capture the rising edge then in interrupt change that register to capture the falling edge of the pulse . 1st store the count value when rising edge is detected and when faling edge is detected minus the current counter from previous counter. this way you can measure the frequency(pulse length).

dhruti

7 replies

waclawek.jan
Super User
April 17, 2020

0693W000000W2bhQAC.png

JW

Tesla DeLorean
Guru
April 18, 2020

There is also an indirect mode allow for a single pin to go to two channels so for example CH1 and CH2 can capture opposite edges.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
berendi
Principal
April 18, 2020

Look up PWM input mode in the reference manual.

DBehe.1
DBehe.1Best answer
Associate
May 12, 2020

At a time you can either capture rising edge or falling edge but there is a solution initially set the register for capture the rising edge then in interrupt change that register to capture the falling edge of the pulse . 1st store the count value when rising edge is detected and when faling edge is detected minus the current counter from previous counter. this way you can measure the frequency(pulse length).

dhruti

bnymntrz
Associate III
May 12, 2020

It is possible to capture the rising and falling edge of the input signal using the Timer unit, our friend who has already shared the recorder above.

Laurent Ca...
Senior III
October 14, 2020

Dear @Domagoj Ciković​ 

Did an answer here help you to solve your problem?

If yes, which one?

If no, did you have still this problem to solve?

Best regards

Laurent Ca...

Laurent Ca...
Senior III
October 20, 2020

Dear @Domagoj Ciković​ 

I guess you don't have to solve this problem anymore, therefore I consider this thread solved and closed.

If not, feel free to reopen it by posting a new answer.

Best regards

Laurent Ca...