STM32G484-EVAL FDCAN works without BRS, gives stuff errors with BRS turned on
FDCAN clock: 80Mhz
I'm using PCAN view to test this, with proper settings (8Mbps data rate,80Mhz clock,Nominal bit rate of 1Mbps). Works when I turn the BRS off in the TxHeader. Shows stuff error messages with Data Field indicated as soon as I turn BRS on.
Init method:
void MX_FDCAN1_Init(void)
{
hfdcan1.Instance = FDCAN1;
hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
hfdcan1.Init.FrameFormat = FDCAN_FRAME_FD_BRS;
hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
hfdcan1.Init.AutoRetransmission = ENABLE;
hfdcan1.Init.TransmitPause = ENABLE;
hfdcan1.Init.ProtocolException = ENABLE;
hfdcan1.Init.NominalPrescaler = 1;
hfdcan1.Init.NominalSyncJumpWidth = 16;
hfdcan1.Init.NominalTimeSeg1 = 63;
hfdcan1.Init.NominalTimeSeg2 = 16;
hfdcan1.Init.DataPrescaler = 1;
hfdcan1.Init.DataSyncJumpWidth = 4;
hfdcan1.Init.DataTimeSeg1 = 5;
hfdcan1.Init.DataTimeSeg2 = 4;
hfdcan1.Init.StdFiltersNbr = 1;
hfdcan1.Init.ExtFiltersNbr = 0;
hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
{
Error_Handler();
}
}
Tx Header:
// /* Prepare Tx Header */
TxHeader.Identifier = 0x111;
TxHeader.IdType = FDCAN_STANDARD_ID;
TxHeader.TxFrameType = FDCAN_DATA_FRAME;
TxHeader.DataLength = FDCAN_DLC_BYTES_8;
TxHeader.ErrorStateIndicator = FDCAN_ESI_PASSIVE;
TxHeader.BitRateSwitch = FDCAN_BRS_ON;
TxHeader.FDFormat = FDCAN_FD_CAN;
TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
TxHeader.MessageMarker = 0x55;
Payload:
Tx_Payload[0] = ubKeyNumber;
ubKeyNumber=ubKeyNumber+1;
Tx_Payload[1] = 0x00;
Tx_Payload[2] = 0x01;
Tx_Payload[3] = 0x00;
Tx_Payload[4] = 0x01;
Tx_Payload[5] = 0x00;
Tx_Payload[6] = 0x01;
Tx_Payload[7] = 0x00;
Tried with the ESI_ACTIVE as well.
Anything obvious that anyone can see here?