Skip to main content
ARoum.1
Visitor II
Mar 27, 2020 1:42 AM UTC
Question

STM32F103C8T6 with 128kb of flash instead of 64? Fake or genuine?

Hi,

I just received 3 bluepill board I ordered from china and, while trying them, I noticed that one of them shows up as having 128kb of flash. However, they all have the same device ID (0x410).

Is this normal or is that chip fake? How can I test if my STM32s are genuine?

Here is a screenshot from the STLink utility when connecting the 128k board:0693W000000UqvOQAS.png

And here is a utility when connecting a normal board:

0693W000000UqvYQAS.png

Hope someone can help :)

Cheers

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
Mar 27, 2020 7:07 AM UTC

Sorry, but people here don't really care - if you want genuine ST parts, you buy them at renown distributors.

But there are still chances you can use the bluepills as you intended, just nobody here would confirm this to you. You may want to read the discussion at https://www.eevblog.com/forum/microcontrollers/cheap-bluepill-very-likely-it-has-fake-stm32-right/150/ perhaps.

JW

Uwe Bonnes
Chief
Mar 27, 2020 10:13 AM UTC

STM32F103x8 and STM32F103xB are the same chip. So the 128k flash are on chip. On a STM32F103xB, the upper 64 kB are fully tested, on a a STM32F103x8 the flash is probably not tested or was tested bad. So if you play with a a STM32F103x8, you can try to use the upper flash. But do not rely on that flash to work right!