Skip to main content
emre
Associate
Mar 25, 2020 6:33 PM UTC
Solved

Why ST25RU3993_Reader_Suite not detect ST25RU3993-EVAL board?

Hi, 

I bought new ST25RU3993-EVAL from Digikey. And download en.STSW-ST25RU001.zip on ST web site.

ST25RU3993_Reader_Suite software Installed to windows7 PC. Also installed FTDI drivers. 

When i put USB cable to PC, Red LED is ON. 

I see new "USB Serial Port(COM16)" on Windows Device Manager.

On the first run ST25RU3993_Reader_Suite software, automatically detect new firmware and update device with ST25RU3993_FW_v2-0-0-0_Eval.bin

Then open again ST25RU3993_Reader_Suite and click "Connect Reader" button. Then Red LED is OFF. 

And software waiting and locked. No response and no any message. 

I tested with different PC and Windows10, but result is same. Not working.

Why is the software not detecting the board?

Thanks.

This topic has been closed for replies.
Cedric Dalban
Cedric DalbanBest answer
ST Employee
Mar 31, 2020 3:14 PM UTC

Hello emre,

apparently the FW update did not pass.

Could you please force it with this procedure:

  • After having connected your board through USB
  • go to Help->Firmware Update (or use Ctrl-F)
  • select appropriate USB COM port
  • select ST25RU3993_FW_v2-0-0-0_Eval.bin for download.

Could you please as well ensure the following bridges are duly connected:

  • J14
  • J20
  • J21
  • J5

regards,

Cedric.

2 replies

Cedric Dalban
Cedric DalbanBest answer
ST Employee
Mar 31, 2020 3:14 PM UTC

Hello emre,

apparently the FW update did not pass.

Could you please force it with this procedure:

  • After having connected your board through USB
  • go to Help->Firmware Update (or use Ctrl-F)
  • select appropriate USB COM port
  • select ST25RU3993_FW_v2-0-0-0_Eval.bin for download.

Could you please as well ensure the following bridges are duly connected:

  • J14
  • J20
  • J21
  • J5

regards,

Cedric.

Cedric Dalban
ST Employee
Apr 30, 2020 2:25 PM UTC

hello,

after double check, only the following jumper is mandatory for correct board connection through USB:

  • J14 (jumper next to the USB connector)

regards,

Cedric.