Skip to main content
tushar_tp
Associate III
Mar 25, 2020 1:49 AM UTC
Solved

GUI not displaying properly for STM32H753I-EVAL with External SDRAM as Frambuffer.

Touch GFX 4.13.0

STM32CubeMX 5.6.0

STM32H7Cube 1.7.0

Board: STM32H753I-EVAL2 (Screen size for reference is 640X480)

I am developing simple GUI application with 2 screens. each screen has one button with label.

Since the V3 template for this board is not available. I going through the route of creating my own template from CubeMX.

FMC clock = 200MHz

LTDC clock = 25 MHz

I am using external SDRAM with double frambuffer.

location of frambuffer

Frambuffer1 = 0xD0000000

Frambuffer2 = 0xD00E1000

attached is the GUI I am getting on my hardware.0693W000000UfNpQAK.jpg

Attached is GUI on my Simulator

0693W000000UiciQAC.jpg

If you notice the Button is only shown Half. I even tried with single buffer but same result.

I am attaching my project for reference.

I am waiting for V3 template available from TouchGFX, hope it gets uploaded very soon.

Thanks

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Mar 31, 2020 2:35 PM UTC

V3 of H743-Eval is up. Check it out!

/Martin

3 replies

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Mar 31, 2020 2:35 PM UTC

V3 of H743-Eval is up. Check it out!

/Martin

tushar_tp
tushar_tpAuthor
Associate III
Mar 31, 2020 3:47 PM UTC

Thanks Martin. It is working now after comparing with V3 template source code.

Martin KJELDSEN
Principal III
Apr 1, 2020 8:11 AM UTC

*Does a little dance* Yay.