Associate II
March 22, 2020
Solved
USB-OTG suspend on connect
- March 22, 2020
- 3 replies
- 1657 views
Hi,
We're using a STM32MP157C on a custom board and trying to get ethernet over USB to work. We have a type B USB connector on the board and when a cable is connected, the USB peripheral seems to get suspended as the logs from dwc2 shows. We've seen that there are patches for forcing sessions to be valid and added "force-b-session-valid" to the DT node. Yet the only thing we see when we connect is the suspend interrupts firing. Any ideas what's going wrong here?
Thanks