Skip to main content
SZENG.1
ST Employee
March 18, 2020
Solved

How to use the CubeMonitor in snapshot mode without trigger supported?

  • March 18, 2020
  • 13 replies
  • 4842 views

I instrumented the code with the supplied code, and it works fine in STM Studio, but when used in CubeMonitor, after started, the dashbord just displays 'Acquisition started, waiting for value'. I've checked the data flow from STLink and found that only 'x' value present in the data payload, but without 'y' value.

Is there a way to trigger the data sample manually? Or supporting trigger is mandatory in snapshot mode?

This topic has been closed for replies.
Best answer by Richard.Chvr

No update since a while, closing the post.

13 replies

Landry
Visitor II
March 18, 2020

Dear SZENG.1,

Did you configure the node "variables" as expected ?

You have to :

-> select your monitored variables from the executable file

->select the snapshot mode (and verify that header address is detected )

-> select ( if you need it, it's not mandatory) a trigger variable and additional parameters of triggering ( value and start mode ).

0693W000000UBQPQA4.png

Please come back to me if it's still not working.

Landry

SZENG.1
SZENG.1Author
ST Employee
March 18, 2020

Hi Landry,

Here is the situation:

The trigger function in the firmware code is not enabled, as it's not required and for saving RAM and ROM space;

The variables should have been configured correctly:

0693W000000UBWXQA4.pngIf the trigger is selected as 'off' like above, ​after clicked 'Start', the dashboard just shows 'waiting for value:

0693W000000UBWwQAO.png

While, if trigger has been selected other than 'off' like below:

0693W000000UBXLQA4.png

the acq in & out will show an error after started:

0693W000000UBXQQA4.png

Landry
Visitor II
March 18, 2020

-Your node "variables" configuration is correct .

-In snapshot mode, the first point sent ( to set the first timestamp ) is an x only value, so this is also correct.( it means that the start is taking into account ).

-When you don't manage the trigger mode in your embedded application , the message "The trigger mode is not supported" is also correct.

So everything seems ok on CubeMonitor side.

Can you link the error output of your "acquisition in" node to debug node to see if you have some messages available ?

thank you

Christophe
ST Employee
April 6, 2020

Hi SZENG.1,

The acquisition doesn’t start because you embedded application you are using (dataAcq files) was modified. The Size of buffer is defined with the formula: #define SNP_TRC_BUFFER_SIZE (50*(SNP_TRC_NB_MAX_WORD_VAR+1)) and unfortunatly Stm32cubemonitor doesn't allow modification on it. If the default buffer size is not enough large, I advice the increase the parameter SNP_TRC_NB_MAX_WORD_VAR (defined at 10 by default).

Mbert.1
Associate II
April 20, 2020

hi, my goal is to verify a variable named "b" which is increased up to 1000 and then reset to zero, the increase takes place via an interrupt that is generated every 100 ns and check on CubeMonitor in snapshot mode the value of the variable.0693W000000W67RQAS.png Inside the installation folder of the CubeMonitor program I found the dataAcq.c and dataAcq.h files. Inside the dataAcq.c file I found that I had to set SNP_TRC_TIMESTAMP_VALUE (with a value between 1 and 1000) and did not modify NP_TRC_BUFFER_SIZE (50 * (SNP_TRC_NB_MAX_WORD_VAR + 1)).0693W000000W66xQAC.png in the dataAcq.h SNP_TRC_NORD_ORD_MAX_ORD_MAR_MAX file.

0693W000000W66dQAC.png

how should these values be determined? In CubeMonitor I found other values to set in the variable medu (sampling frequenty, trigger treshord). how can i determine these values?0693W000000W67HQAS.png

Mbert.1
Associate II
May 8, 2020

I need to understand how to set SNP_TRC_BUFFER_SIZE in order to display 100 points on the STM STUDIO, setting the quantity of variables to 9 (SNP_TRC_NB_MAX_WORD_VAR = 9). In STM STUDIO I set the Start in (Manual) and the Stop (when buffer full). if I set SNP_TRC_BUFFER_SIZE (10 * (SNP_TRC_NB_MAX_WORD_VAR + 1)) I don't find myself in STM STUDIO 100 points but I find myself with 32 points. How can I get 100 points, how should the variables be set.

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
September 27, 2023

No update since a while, closing the post.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.