Skip to main content
kumar singh
Associate II
March 17, 2020
Solved

How to flash external target(SPC560B50L5C6E0Y) using SPC560B-DIS dev kit

  • March 17, 2020
  • 3 replies
  • 1830 views

Hi, We are using SPC560B50L5C6E0Y microcontroller for one of our application. I have SPC560B-DIS with me and want to flash want to flash SPC560B50L5C6E0Y controller in our designed board. I want to know the required jumper setting on dev kit for flashing external target. What settings on SPC560B-DIS kit decides whether to flash the on-board controller or external target? I have removed S1,S2 jumpers and powering through USB. I have placed J19,J20 jumper and trying to flash but controller is not getting flashed correctly.

    This topic has been closed for replies.
    Best answer by Erwan YVIN

    Hello Kumar ,

    Did you solve your issue ?

    I think that it is possible to flash SPC560B50L5C6E0Y using SPC560B-DIS dev kit

    You can use LINFlex cf chapter 5.2.2 of RM0017 in order to flash

    Best Regards

    Erwan

    3 replies

    kumar singh
    Associate II
    March 18, 2020

    Hi, I am able to flash SPC560B60L5B6E0Y based external target using discovery kit and it functions correctly as per developed firmware. Programming succeeds in flashing SPC560B50L5C6E0Y controller but the hardware is not responding as per code it should. I am trying to toggle the gpio but its not toggling. I want to know if discovery kit can be used to flash the SPC560B50L5C6E0Y target. Also how does discovery kit decides whether to flash the on-board target or external target. JTAG lines in discovery kit is sharing with on-board controller as well as. So will my external target get programmed if the on-board and external targets are different?

    Erwan YVIN
    Erwan YVINBest answer
    ST Technical Moderator
    April 1, 2020

    Hello Kumar ,

    Did you solve your issue ?

    I think that it is possible to flash SPC560B50L5C6E0Y using SPC560B-DIS dev kit

    You can use LINFlex cf chapter 5.2.2 of RM0017 in order to flash

    Best Regards

    Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    kumar singh
    Associate II
    April 1, 2020

    Hi Erwan,

    Yes, i am able to flash using JTAG interface.

    Regards

    kumar