Skip to main content
IDANI.1
Visitor II
March 17, 2020
Question

stm uart communication voltage

  • March 17, 2020
  • 1 reply
  • 2578 views

I want to use stm32f407gt with nextion touch screen. Display and stm will connect via to uart(Rx Tx pins). Stm work with 3.3V and nextion works with 5V. It will effect to communication ?

This topic has been closed for replies.

1 reply

KnarfB
Super User
March 17, 2020

STM app note AN4899:

"If the 5V UART interface input is TTL compatible, VOL<0.8V and VOH>2.0V. This implies that a 3.3V CMOS output can drive without any problem. An STM32 FT pad can accept 0V to 5V CMOS level input when VDD=3.3V."

FT = 5V tolerant pad.