Question
STM32 ADC power supply
Customer asks me to use STM32 powered from 3.3V with ADC reference 3.3V too (different source). So there is two possibel topologies:
- Connect VDD and VDDA, use precision source for VREF
- Connect VDDA and VREF to precision source, VDD connect to standard source.
In the DS I didnt found clear info about this:
"A maximum difference of 300 mV between VDD and VDDA can be tolerated during power-up and power-down operation"
"VDDA Must be the same potential as VDD"
"The voltage on VREF+ may range between 2.4 V and VDDA"
In my case, standard 3.3V source can differ +/-200mV from reference 3.3V source. Is it acceptable to use STM32F405 this way?