Skip to main content
Takemasa
Associate III
March 14, 2020
Question

I2C module is excessively generated by CubeIDE

  • March 14, 2020
  • 1 reply
  • 1137 views

Overview

While the I2C module is enabled by CubeIDE Device Configuration Tool,

  • CubeIDE 1.3.0
  • Nucleo H743ZI
  • HAL FW 1.7.0

Reproduce the problem

Follow :

  1.  Create a new Nucleo H743ZI project
  2.  Generate the code from the Device Configuration Tool as default condition (All I2C are disabled)
  3.  You can find Drivers/STM32H7xx_HAL_Driver/Inc/stm32h7xx_hal_i2c.h while I2C is not chosen in the Device Configuration Tool.

This excessive I2C generation define a HAL_I2C_MODULE_ENABLED incorrectly, and it interferes the program which have IFDEF block with HAL_I2C_MODULE_ENABLED.

Demonstration of the problem

This problem can be demonstrated by the d009-nucleo-h743rb-i2c project inside attached d009.zip. This program doesn't have I2C as configured module. And this has following code in the main() function.

 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_RESET);
#ifdef HAL_I2C_MODULE_ENABLED
 // In this project, we don enable I2C by CubeIDE configuration.
 // So, if the following code is executed, project is incorrectly configured.
 HAL_GPIO_WritePin(LD3_GPIO_Port, LD3_Pin, GPIO_PIN_SET);
#endif

Thus, if LED is turned on, that is sign of the excessive I2C module. And you can see the LED is on if you run it on Nucleo.

Note that the d009-nucleo-g431rb-control has same logic as above, but LED is not turned on, if you run it on Nucleo G431RB. So there is no excessive I2C module issue for STM32G431

Others

I saw same problem for Nucleo L152 and Nucleo F091.

This topic has been closed for replies.

1 reply

Khouloud ZEMMELI
ST Employee
March 25, 2020

​Hello @Takemasa​ ,

This will be internally checked.

Best Regards,

Khouloud