Skip to main content
jefazo92
Associate III
March 14, 2020
Solved

Makefile:44 Error 1

  • March 14, 2020
  • 9 replies
  • 13508 views

Hi everyone,

I have just created a project. I haven't done any modifications and I am getting this error when building the project:

make: *** [makefile:44: nucleo-g474re-blinky.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
 
19:26:10 Build Failed. 1 errors, 0 warnings. (took 1s.74ms)

Could someone help me out ? Thanks in advance.

This topic has been closed for replies.
Best answer by KnarfB

The root cause error is "STM32G474RETX_FLASH.ld: No such file or directory"

Does this file exist? It should have been generated with the project.

My guess: its a problem with your project path "C:\Users\Gonzalo Andaluc??a\..."

Eclipse is notorious for having issues with non-ASCII letters, space, .... Try a simple path like C:\test1

9 replies

KnarfB
Super User
March 14, 2020

44 only means line 44 in makefile. There should be more output in the console log indicating errors/warnings...

jefazo92
jefazo92Author
Associate III
March 14, 2020
20:30:54 **** Incremental Build of configuration Debug for project AkunaMatata ****
make -j8 all 
arm-none-eabi-gcc "../Core/Src/main.c" -mcpu=cortex-m4 -std=gnu11 -g3 -DUSE_HAL_DRIVER -DSTM32G474xx -DDEBUG -c -I../Drivers/STM32G4xx_HAL_Driver/Inc/Legacy -I../Drivers/CMSIS/Include -I../Drivers/CMSIS/Device/ST/STM32G4xx/Include -I../Core/Inc -I../Drivers/STM32G4xx_HAL_Driver/Inc -O0 -ffunction-sections -fdata-sections -Wall -fstack-usage -MMD -MP -MF"Core/Src/main.d" -MT"Core/Src/main.o" --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -o "Core/Src/main.o"
arm-none-eabi-gcc -o "AkunaMatata.elf" @"objects.list" -mcpu=cortex-m4 -T"C:\Users\Gonzalo Andalucía\STM32CubeIDE\workspace_1.3.0\AkunaMatata\STM32G474RETX_FLASH.ld" --specs=nosys.specs -Wl,-Map="AkunaMatata.map" -Wl,--gc-sections -static --specs=nano.specs -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -Wl,--start-group -lc -lm -Wl,--end-group
c:\st\stm32cubeide_1.3.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\arm-none-eabi\bin\ld.exe: cannot open linker script file C:\Users\Gonzalo Andaluc??a\STM32CubeIDE\workspace_1.3.0\AkunaMatata\STM32G474RETX_FLASH.ld: No such file or directory
collect2.exe: error: ld returned 1 exit status
make: *** [makefile:44: AkunaMatata.elf] Error 1
"make -j8 all" terminated with exit code 2. Build might be incomplete.
 
20:30:55 Build Failed. 1 errors, 0 warnings. (took 1s.418ms)

Thanks for replying @KnarfB​ . This is all I'm getting.

jefazo92
jefazo92Author
Associate III
March 14, 2020

0693W000000TwIuQAK.png

KnarfB
KnarfBBest answer
Super User
March 14, 2020

The root cause error is "STM32G474RETX_FLASH.ld: No such file or directory"

Does this file exist? It should have been generated with the project.

My guess: its a problem with your project path "C:\Users\Gonzalo Andaluc??a\..."

Eclipse is notorious for having issues with non-ASCII letters, space, .... Try a simple path like C:\test1

jefazo92
jefazo92Author
Associate III
March 15, 2020

@KnarfB​  THANK YOU FOR SAVING MY LIFE. YOU ARE MY HERO.You were right, the accent was causing all the trouble so I had to rename my user folder. Then I uninstalled and reinstalled the program and now I have finally been able to upload my first program into my MCU.

jefazo92
jefazo92Author
Associate III
March 14, 2020

How can I do this @KnarfB​  ? Do I just create another folder in C:\Users ? And paste the CubeIDE folder into it ?

jefazo92
jefazo92Author
Associate III
March 14, 2020

Ok. I did it that way but did not solve anything. I will try to uninstall it and instal it again but now I'll instal the program in the new folder with ASCCII characters.

SMath.2
Visitor II
June 14, 2020

The issue got resolved when I renamed my project without any numerical. eg John1 to john. the path is still the same. I understand this is illogical fix, but worked for me, would be nice if someone got a valid explanation for this!! thanks

BRoel.1
Visitor II
January 24, 2021

For me the same error was caused by a seemingly unrelated 'unknown type' error that showed after the makefile error 1 in the problems window.

Checking the console window would've helped: it showed the actual cause first.