Skip to main content
DRobe.4
Associate III
March 12, 2020
Solved

EXTI PI2 not working on STM327508-DK

  • March 12, 2020
  • 3 replies
  • 760 views

I have viewed every example on the internet, I think and seen many different commands and approaches. As long as the interrupt is disabled, the program works, but it crashes when enabled. Here are snippets related to EXTI. Maybe I have mixed code from too many sources and something conflicts.

   RCC->APB2ENR |= RCC_APB2ENR_SYSCFGEN;

  __HAL_RCC_GPIOI_CLK_ENABLE();

      GPIO_InitStruct.Mode       = GPIO_MODE_INPUT;

//   GPIO_InitStruct.Mode       = GPIO_MODE_IT_RISING;

      GPIO_InitStruct.Pull         = GPIO_PULLUP;                        

      GPIO_InitStruct.Pin        = GPIO_PIN_2;

      GPIO_InitStruct.Speed      = GPIO_SPEED_LOW;

      HAL_GPIO_Init(GPIOI, &GPIO_InitStruct);

      HAL_NVIC_SetPriority(EXTI2_IRQn, 2, 3);                           

      NVIC_EnableIRQ(EXTI2_IRQn);

   EXTI->IMR |= 1<<2;                                                         

   EXTI->RTSR |= 1<<2;                                                         // Enable the 'rising edge' trigger (button release)

   SYSCFG->EXTICR[0] = 0x800;                                             // EXTICR[0] is EXTICR1. Line2 is 3rd set of 4 bits, PortI is 8th port starting with A

void EXTI2_IRQHandler(void)

{

   if (EXTI->PR & (1<<2))

    {

     EXTI->PR |= (1<<2);                                                         // Clear the EXTI status flag

//     NVIC_ClearPendingIRQ(EXTI2_IRQn);                               // Clear previous interrupt in NVIC

    HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1);                        // Toggle PI1

      }

}

.

This topic has been closed for replies.
Best answer by Tesla DeLorean

Define "crash", when you stop in the debugger WHERE is it?

If in the Default Handler that would suggest the linker isn't binding the one you have supplied.

Is this using a .CPP or compiled as C++ ? If so use extern "C" so the name isn't mangled.

Try writing this in consistent HAL form, I'm not looking to unpack the bit fields and registers.

extern "C" void EXTI2_IRQHandler(void)
{
 /* EXTI line interrupt detected */
 if(__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_2) != RESET)
 {
 __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_2);
 HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1); // Toggle PI1
 }
}
 
 
static void EXTI2_IRQHandler_Config(void)
{
 GPIO_InitTypeDef GPIO_InitStructure = {0};
 
 /* Enable GPIOI clock */
 __HAL_RCC_GPIOI_CLK_ENABLE();
 
 /* Configure PI.2 pin as input floating */
 GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStructure.Pull = GPIO_NOPULL;
 GPIO_InitStructure.Pin = GPIO_PIN_2;
 HAL_GPIO_Init(GPIOI, &GPIO_InitStructure);
 
 /* Enable and set EXTI lines 2 Interrupt to the lowest priority */
 HAL_NVIC_SetPriority(EXTI2_IRQn, 2, 0);
 HAL_NVIC_EnableIRQ(EXTI2_IRQn);
}

3 replies

Tesla DeLorean
Tesla DeLoreanBest answer
Guru
March 12, 2020

Define "crash", when you stop in the debugger WHERE is it?

If in the Default Handler that would suggest the linker isn't binding the one you have supplied.

Is this using a .CPP or compiled as C++ ? If so use extern "C" so the name isn't mangled.

Try writing this in consistent HAL form, I'm not looking to unpack the bit fields and registers.

extern "C" void EXTI2_IRQHandler(void)
{
 /* EXTI line interrupt detected */
 if(__HAL_GPIO_EXTI_GET_IT(GPIO_PIN_2) != RESET)
 {
 __HAL_GPIO_EXTI_CLEAR_IT(GPIO_PIN_2);
 HAL_GPIO_TogglePin(GPIOI, GPIO_PIN_1); // Toggle PI1
 }
}
 
 
static void EXTI2_IRQHandler_Config(void)
{
 GPIO_InitTypeDef GPIO_InitStructure = {0};
 
 /* Enable GPIOI clock */
 __HAL_RCC_GPIOI_CLK_ENABLE();
 
 /* Configure PI.2 pin as input floating */
 GPIO_InitStructure.Mode = GPIO_MODE_IT_RISING;
 GPIO_InitStructure.Pull = GPIO_NOPULL;
 GPIO_InitStructure.Pin = GPIO_PIN_2;
 HAL_GPIO_Init(GPIOI, &GPIO_InitStructure);
 
 /* Enable and set EXTI lines 2 Interrupt to the lowest priority */
 HAL_NVIC_SetPriority(EXTI2_IRQn, 2, 0);
 HAL_NVIC_EnableIRQ(EXTI2_IRQn);
}

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
DRobe.4
DRobe.4Author
Associate III
March 12, 2020

Clive, you did it! and your approach avoids the messy SYSCFG code which comes in 100 flavours on the internet. Thank you!

dbgarasiya
Senior
March 12, 2020

great