Skip to main content
STobo.1
Associate
Mar 12, 2020 12:21 AM UTC
Question

4ch adc records on sd card

Hello,

I try make a program for record on sd card a data/values from 4 channels adc1.

First I make program for read a 4 channels from adc1 and it works!

When I pause a debug in while loop, in uint32_t adc[4] I have all 4 correct values.

Then I make a program for write some data to sd card it works!

When I check sd card on pc; after debug; I have new file.txt with data ;)

So when I just make active a adc1 in cubemx for sdcardonly project and try run in on truestudio, nothing with previous issues works! -.-...............

sdcardplus4chadc attachments

#include "main.h"
#include "fatfs.h"
 
ADC_HandleTypeDef hadc1;
DMA_HandleTypeDef hdma_adc1;
 
SD_HandleTypeDef hsd;
 
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_SDIO_SD_Init(void);
static void MX_ADC1_Init(void);
 
uint32_t adc[4], buffer[4];
 
long long k=0;
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)
{
	for (int i =0; i<4; i++)
	{
	 adc[i] = buffer[i]; // store the values in adc[]
	 k++;
	}
 
}
 
int main(void)
{
 
 HAL_Init();
 
 SystemClock_Config();
 
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_SDIO_SD_Init();
 MX_FATFS_Init();
 MX_ADC1_Init();
 
 FATFS myFATAFS;
 FIL myFILE;
 UINT testByte;
 
 if(f_mount(&myFATAFS, SDPath, 1) == FR_OK)
 {
 
 char myPath[]="sdcardplus.txt\0";
 f_open(&myFILE, myPath, FA_WRITE | FA_CREATE_ALWAYS);
 char myData[]="HELLO\0";
 f_write(&myFILE, myData, sizeof(myData), &testByte);
 f_close(&myFILE);
 }
 
 while (1)
 {
		HAL_ADC_Start_DMA(&hadc1, buffer, 4);
	 	HAL_Delay (1000);
	 	HAL_ADC_Stop_DMA(&hadc1);
	 	HAL_Delay (1000);
	 	k=0;
 }
}
 
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
 
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
 
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
 RCC_OscInitStruct.HSEState = RCC_HSE_ON;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 168;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 4;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
 
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
 
 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2) != HAL_OK)
 {
 Error_Handler();
 }
}
 
static void MX_ADC1_Init(void)
{
 
 ADC_ChannelConfTypeDef sConfig = {0};
 
 hadc1.Instance = ADC1;
 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
 hadc1.Init.Resolution = ADC_RESOLUTION_12B;
 hadc1.Init.ScanConvMode = ENABLE;
 hadc1.Init.ContinuousConvMode = ENABLE;
 hadc1.Init.DiscontinuousConvMode = DISABLE;
 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc1.Init.NbrOfConversion = 4;
 hadc1.Init.DMAContinuousRequests = ENABLE;
 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
 if (HAL_ADC_Init(&hadc1) != HAL_OK)
 {
 Error_Handler();
 }
 
 sConfig.Channel = ADC_CHANNEL_1;
 sConfig.Rank = 1;
 sConfig.SamplingTime = ADC_SAMPLETIME_28CYCLES;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sConfig.Channel = ADC_CHANNEL_2;
 sConfig.Rank = 2;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sConfig.Channel = ADC_CHANNEL_3;
 sConfig.Rank = 3;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
 sConfig.Channel = ADC_CHANNEL_8;
 sConfig.Rank = 4;
 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 
}
 
static void MX_SDIO_SD_Init(void)
{
 
 hsd.Instance = SDIO;
 hsd.Init.ClockEdge = SDIO_CLOCK_EDGE_RISING;
 hsd.Init.ClockBypass = SDIO_CLOCK_BYPASS_DISABLE;
 hsd.Init.ClockPowerSave = SDIO_CLOCK_POWER_SAVE_DISABLE;
 hsd.Init.BusWide = SDIO_BUS_WIDE_1B;
 hsd.Init.HardwareFlowControl = SDIO_HARDWARE_FLOW_CONTROL_DISABLE;
 hsd.Init.ClockDiv = 0;
 
}
 
static void MX_DMA_Init(void) 
{
 
 __HAL_RCC_DMA2_CLK_ENABLE();
 
 HAL_NVIC_SetPriority(DMA2_Stream0_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA2_Stream0_IRQn);
 
}
static void MX_GPIO_Init(void)
{
 
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOD_CLK_ENABLE();
 
}
 
void Error_Handler(void)
{
 
}
 
#ifdef USE_FULL_ASSERT
 
void assert_failed(uint8_t *file, uint32_t line)
{ 
 
}
#endif
 

Please help me or just give me some clue.

Best Regards

Szymon

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Mar 12, 2020 1:33 AM UTC

Use a merge tool, and make sure you've pulled over all MSP initialization code, as well as all interrupt code

Too many files attached.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
STobo.1
STobo.1Author
Associate
Mar 12, 2020 7:19 AM UTC

look at now ;)