ADC to DAC using DMA
If I set my sine wave generator to 1.5 Vpk-pk the DAC outputs a nice clean sine wave. If I increase the ADC input above that level, I start to see clipping of the sine wave. The negative part of the wave begins clipping before the positive part. Is the clipping cause because the DAC doesn't need the full 3 volt pk-pk input internally from the DMA to output a 3 volt pk-pk signal?
My ultimate goal is to transfer the sine wave signal to the Ethernet engine for transmission over the network. When I do that I assume I will need to input a 3 Vpk-pk signal to take full advantage of the ADC conversion. Is that correct?
I have two STM32F4 Discovery boards that I will be using for this project. I have the ADC to DAC working on one of them. My next step is to set both boards up and get them to communicate over the network with each other. Once that is done I will input the sine wave into ADC1 on board one and send it out over the network. Board two will then receive the data and pass it on to its DAC module (hopefully).