Skip to main content
BSpoe.1
Associate III
March 10, 2020
Question

STM32WB55 Device Name is not changed in GAP/GATT

  • March 10, 2020
  • 4 replies
  • 1914 views

Hey,

I try to change the device name for my broadcast inside the initialization of the Ble_Hci_Gap_Gatt_Init() funtion. My implementation is the following:

static void Ble_Hci_Gap_Gatt_Init(void){
 
 uint8_t index;
 uint16_t gap_service_handle, gap_dev_name_char_handle, gap_appearance_char_handle;
 const uint8_t *bd_addr;
 uint16_t appearance[1] = { BLE_CFG_GAP_APPEARANCE }; 
 
 /**
 * Initialize HCI layer
 */
 /*HCI Reset to synchronise BLE Stack*/
 hci_reset();
 
 /**
 * Write the BD Address
 */
 
 bd_addr = BleGetBdAddress();
 aci_hal_write_config_data(CONFIG_DATA_PUBADDR_OFFSET, 
 CONFIG_DATA_PUBADDR_LEN, 
 (uint8_t*) bd_addr
 );
 
 /**
 * Set TX Power to 0dBm.
 */
 aci_hal_set_tx_power_level(1, CFG_TX_POWER);
 
 /**
 * Initialize GATT interface
 */
 aci_gatt_init();
 
 /**
 * Initialize GAP interface
 */
 const char *name = "STM32WB";
 aci_gap_init(GAP_PERIPHERAL_ROLE, 
 0, 
 APPBLE_GAP_DEVICE_NAME_LENGTH, 
 &gap_service_handle, 
 &gap_dev_name_char_handle, 
 &gap_appearance_char_handle
 );
 
 if (aci_gatt_update_char_value(gap_service_handle, 
 gap_dev_name_char_handle, 
 0,
 strlen(name), 
 (uint8_t *) name))
	{
	 BLE_DBG_SVCCTL_MSG("Device Name aci_gatt_update_char_value failed.\n");
	}
 
 if(aci_gatt_update_char_value(gap_service_handle,
 gap_appearance_char_handle,
 0,
 2,
 (uint8_t *)&appearance))
 {
 BLE_DBG_SVCCTL_MSG("Appearance aci_gatt_update_char_value failed.\n");
 }
/**
 * Initialize Default PHY
 */
 hci_le_set_default_phy(ALL_PHYS_PREFERENCE,TX_1M,RX_1M);
 
}

With the debugger I can see that every function returns a BLE_SUCCESS, but nothing is changed. My BLE scanner app shows me "P2PSRV1" as the device name.

What can I do to set the correct name?

Thanks a lot,

Ben

This topic has been closed for replies.

4 replies

AClif
Associate III
April 7, 2020

I am having the exact same problem, did you manage to get this working?

KPrzy.1
Associate II
September 8, 2021

did You solved this isse? I noticed that when I am changing example then name change but when build two times application with two times name change the name stay unchanged

tguly.1
Associate II
March 10, 2023

Ran into the same issue. Any comment, solution on this one?

tguly.1
Associate II
March 10, 2023