Problem with downloads to STM32F746G DISCO and TouchGFX demonstration program from FW F7 V1.16.0 repository
Hello,
demo project is prepared for SW4ST32. After importing I can build all files without any problem.
Then trying download (by Debug option from menu) I have achived some problems - but it seems that is flasded. On DISCO there is nothing until reset button is pressed. I can see very distorion pitures from those demo example , there is some interaction with touch . I think BSP works fine, but there is some problem during downloads.
Does SW4ST32 using STLINK rcognizes that part of code is for internal flash and other for QSPI? O rather should user declare segments for two hex files and use external programming tool?
Piotr