Skip to main content
PWilk.2
Associate II
March 4, 2020
Solved

How to configure HDMI in openstlinux_eglfs st-example-image-qt image running on STM32MP157C-DK2

  • March 4, 2020
  • 2 replies
  • 2668 views

I need to connect a Waveshare Electronics 5.5" HDMI AMOLED display that does not provide it's supported modes, their website states it needs to be configured manually with the following

max_framebuffer_height=1920

max_usb_current=1

config_hdmi_boost=10

hdmi_group=2

hdmi_force_hotplug=1

hdmi_mode=87

hdmi_timings=1080 1 26 4 50 1920 1 8 2 6 0 0 0 60 0 135580000 3

How would I do this on the openstlinux_eglfs st-example-image-qt image ?

Thanks in advance.

This topic has been closed for replies.
Best answer by KChar.1

After a few trial and error attempts and with some great ST guides I was able to figure this out. I am sharing the solution to this issue for anyone else that might find this useful.

First for the permission issue on the modetest. In wenston distros the weston@root.service has to be stoped. In eglfs there is no weston service. In order to run a modetest the framebuffer has to be empty. In my case was the psplash-drm example that was running.

root@stm32mp1:~# modetest -M stm -s 32:480x1920 
setting mode 480x1920-60.00Hz@XR24 on connectors 32, crtc 35
failed to set mode: Permission denied

Stoping the example (or any other eglfs/qt application) will free the framebuffer for modetest

psplash-drm-quit

The main issue in my case was the clock as indicated by @PatrickF​ . The display needed a 79MHz pixel clock. The MP1 can support up to 90MHz as indicated in the FAQ but the default configuration for DK1 and DK2 boards is 74MHz. So changing the clock worked as intended. To change the clock I created a custom image in cubeMX and compiled it as described in this guide.

2 replies

PatrickF
ST Employee
March 5, 2020

Please see https://wiki.st.com/stm32mpu/wiki/How_to_display_on_HDMI

You should use "modetest -M stm" to retrieve all modes provided by your display.

We do not support 135.58MHz pixel clock as stated in the hdmi_timings above, so if your display does not have lower frame rate mode which fit with 74.25MHz pixel clock (e.g. 30fps), there is no chances that your full HD (1920x1080) display could work.

Note also as stated in the wiki, that 1920x1080 might not work properly in all of your use cases as on DK2 the DDR is only 16-bits and CPU/GPU might not have enough performances.

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent
PWilk.2
PWilk.2Author
Associate II
March 5, 2020

Thank you Patrick.

Unfortunately modetest does not return any display modes for this display, see output below.

I've contacted the supplier to obtain what display modes it does support.

The link you kindly provided shows how to manually configure Weston using /etc/xdg/weston/weston.ini, assuming the display supplier provides the display mode info for this AMOLED display, how would one manually configure eglfs to support alternate modes ?

# modetest -M stm

Encoders:

id     crtc   type   possible crtcs possible clones

28     0      DPI    0x00000001     0x00000000

Connectors:

id     encoder status         name           size (mm)      modes  encoders

29     0      connected      HDMI-A-1       0x0            0      28

 props:

       1 EDID:

               flags: immutable blob

               blobs:

               value:

                       00ffffffffffff002194333400888888

                       1c1c0103800000780a0dc9a057479827

                       12484c00000001010101010101010101

                       010101010101b8353868408010702020

                       8400803874000018b835386840801070

                       20208400803874000018000000fc0054

                       3737392d3130387831393230000000fd

                       00147801ff1d000a202020202020016f

                       02031a7147c646464646464623090701

                       8301000065030c001000b83538684080

                       107020208400803874000018b8353868

                       4080107020208400803874000018b835

                       38684080107020208400803874000018

                       b8353868408010702020840080387400

                       00180000000000000000000000000000

                       0000000000000000000000000000002f

       2 DPMS:

               flags: enum

               enums: On=0 Standby=1 Suspend=2 Off=3

               value: 0

       5 link-status:

               flags: enum

               enums: Good=0 Bad=1

               value: 0

       6 non-desktop:

               flags: immutable range

               values: 0 1

               value: 0

       19 CRTC_ID:

               flags: object

               value: 0

CRTCs:

.

.

.

and on an STM32MP157A-DK1 running stock Linux OS with Weston :-

root@stm32mp1:~# echo 4 > /sys/module/drm/parameters/debug

root@stm32mp1:~# systemctl restart weston

root@stm32mp1:~# dmesg

[ 499.441942] Gcnano is present and activated

[ 500.162116] [drm:drm_helper_probe_single_connector_modes] [CONNECTOR:29:HDMI-A-1]

[ 500.200736] [drm:drm_add_display_info] non_desktop set to 0

[ 500.200758] [drm:drm_add_display_info] HDMI: DVI dual 0, max TMDS clock 0 kHz

[ 500.200807] [drm:drm_add_edid_modes.part.19] ELD monitor T779-108x1920

[ 500.200827] [drm:drm_add_edid_modes.part.19] HDMI: latency present 0 0, video latency 0 0, audio latency 0 0

[ 500.200841] [drm:drm_add_edid_modes.part.19] ELD size 36, SAD count 1

[ 500.200854] [drm:drm_add_display_info] non_desktop set to 0

[ 500.200866] [drm:drm_add_display_info] HDMI: DVI dual 0, max TMDS clock 0 kHz

[ 500.202072] [drm:drm_mode_debug_printmodeline] Modeline 33:"1080x1920" 60 137520 1080 1112 1144 1184 1920 1928 1932 1936 0x48 0xa

[ 500.202088] [drm:drm_mode_prune_invalid] Not using 1080x1920 mode: CLOCK_HIGH

[ 500.202110] [drm:drm_mode_debug_printmodeline] Modeline 40:"1280x720" 0 148500 1280 1720 1760 1980 720 725 730 750 0x40 0x5

[ 500.202122] [drm:drm_mode_prune_invalid] Not using 1280x720 mode: CLOCK_HIGH

Best,

Paul.

KChar.1
Senior
November 10, 2021

Hi @wpaulilkinson​  and @PatrickF​,

I know that its been a while but is there any chance that you figured this out?

I am facing a similar issue. I have a display with particular specifications that I want to configure in ostl-eglfs. I have already configured it to run on a rPi with the following settings. I made sure that my timings are compatible with STM32MP157D-DK1 according to this article. Our display will need 79MHz which seems within spec.

DISPLAY Specs: 
 
hdmi_pixel_freq_limit=400000000
hdmi_timings=480 0 70 35 45 1920 0 12 2 2 0 0 0 60 0 73180000 0
hdmi_drive=2
disable_overscan=1
max_framebuffer_width=2560
max_framebuffer_height=2560
display_rotate=3
framebuffer_width=1920
framebuffer_height=480
hdmi_aspect_21_9=7
hdmi_mode=87
hdmi_group=2
hdmi_ignore_edid=0xa5000080

Modetest returns one mode available but the screen remains unresponsive. The 0x0 size on the connector does not look very promising either.

Connectors:
id	encoder	status		name		size (mm)	modes	encoders
32	31	connected	HDMI-A-1 	0x0		1	31
 modes:
	index name refresh (Hz) hdisp hss hse htot vdisp vss vse vtot)
 #0 480x1920 60.00 480 550 585 630 1920 1932 1934 1936 73180 flags: nhsync, nvsync; type: preferred, driver
 

When I am trying to set this mode I get a permission denied error. The weston@root.service as indicated in this wiki page does not exist in EGLFS.

root@stm32mp1:~# systemctl stop weston@root.service
Failed to stop weston@root.service: Unit weston@root.service not loaded.
 
root@stm32mp1:~# modetest -M stm -s 32:480x1920 
setting mode 480x1920-60.00Hz@XR24 on connectors 32, crtc 35
failed to set mode: Permission denied
 

Following the suggested article it seems that /etc/xdg/weston/weston.ini does not exist in eglfs either.

Any advice or help will be highly appreciated

KChar.1
KChar.1Best answer
Senior
November 30, 2021

After a few trial and error attempts and with some great ST guides I was able to figure this out. I am sharing the solution to this issue for anyone else that might find this useful.

First for the permission issue on the modetest. In wenston distros the weston@root.service has to be stoped. In eglfs there is no weston service. In order to run a modetest the framebuffer has to be empty. In my case was the psplash-drm example that was running.

root@stm32mp1:~# modetest -M stm -s 32:480x1920 
setting mode 480x1920-60.00Hz@XR24 on connectors 32, crtc 35
failed to set mode: Permission denied

Stoping the example (or any other eglfs/qt application) will free the framebuffer for modetest

psplash-drm-quit

The main issue in my case was the clock as indicated by @PatrickF​ . The display needed a 79MHz pixel clock. The MP1 can support up to 90MHz as indicated in the FAQ but the default configuration for DK1 and DK2 boards is 74MHz. So changing the clock worked as intended. To change the clock I created a custom image in cubeMX and compiled it as described in this guide.