ST25RU3993-EVAL: I can't switch to internal PA => TX setting failed
I'm running a ST25RU3993-EVAL with firmware version V2.0.0.0 STUHFL. Under "Reader Settings" in tab "Settings" under "EU Profile", within the TX-Options, there is a Selection-Field "Internal/External PA", which by default is set to external PA.
When I try to set this to internal PA, I do get an error message "TX setting failed".
Has anyone an idea, if this feature is possibly disabled by firmware, or even not yet implemented?