Skip to main content
rudy
Visitor II
March 2, 2020
Question

STM32H743 Nucleo Board ADC-DMA and UART-DMA receive problem?

  • March 2, 2020
  • 0 replies
  • 782 views

I am using STM32H743 nucleo board for the purposes mentioned below. I create the project using Cubemx version 5.3.0 and STM firmware is 1.6.0

* Creating TTL Output signals

* Reading TTL Input Signals

*UART-DMA Receive&Transmit

*PWM (100us PW, 1ms Period)

*ADC-DMA ( Detecting analog signals.) (One-shot 1000 byte data)

I used UART with DMA both tx and rx modes. If I dont use ADC-DMA, everthing works correctly without any fault. I send 10byte data to MCU via FTDI converter. All peripherals work as expected.

When I send a command in order to start HAL_ADC_Start_DMA, hard fault occurs. I tried to debug and I saw that ADC takes datas to buffer correctly but then HAL_UART_Receive_DMA does not work correctly because it is busy all time so system gives hard fault.

I attached main, it and msp.c files. Thanks for your support.

This topic has been closed for replies.