Skip to main content
March 1, 2020
Question

How to activate debug messages for LWIP?

  • March 1, 2020
  • 1 reply
  • 5462 views

I was able to activate the messages for USB Host, but I am not able for LWIP, it seems that there is a specific combination of options, so that messages are enabled

Thank you.

/** Enable debug message printing, but only if debug message type is enabled
 * AND is of correct type AND is at least LWIP_DBG_LEVEL.
 */
#ifdef __DOXYGEN__
#define LWIP_DEBUG
#undef LWIP_DEBUG
#endif
 
#ifdef LWIP_DEBUG
#define LWIP_DEBUGF(debug, message) do { \
 if ( \
 ((debug) & LWIP_DBG_ON) && \
 ((debug) & LWIP_DBG_TYPES_ON) && \
 ((s16_t)((debug) & LWIP_DBG_MASK_LEVEL) >= LWIP_DBG_MIN_LEVEL)) { \
 LWIP_PLATFORM_DIAG(message); \
 if ((debug) & LWIP_DBG_HALT) { \
 while(1); \
 } \
 } \
 } while(0)
 
#else /* LWIP_DEBUG */
#define LWIP_DEBUGF(debug, message)
#endif /* LWIP_DEBUG */

0690X00000DYNnfQAH.png

This topic has been closed for replies.

1 reply

alister
Senior III
March 1, 2020

Add to your lwipopts.h,

#define LWIP_DEBUG 0
//#define NETIF_DEBUG LWIP_DBG_ON
//#define DHCP_DEBUG LWIP_DBG_ON
//#define UDP_DEBUG LWIP_DBG_ON
//#define MEMP_DEBUG LWIP_DBG_ON
//#define MEM_DEBUG LWIP_DBG_ON
//#define ICMP_DEBUG LWIP_DBG_ON

Uncomment whichever topic you want logging.