Skip to main content
pbayton9
Associate II
February 27, 2020
Question

Effect of timer CCR not in range 0
  • February 27, 2020
  • 2 replies
  • 900 views

DMA requests are still generated if the CCR is outside the auto-reload range

The DMA request is is generated when CNT reaches 0 rather than being disabled.

Processor is a STM32H750

is this a bug or a feature - it should be documented anyway

This topic has been closed for replies.

2 replies

waclawek.jan
Super User
February 27, 2020

This is a known, documented, albeit admittedly surprising behaviour (it has been discussed on this forum several times).

Note, that DMA requests are consequence of the event which sets the CCxIF flag.

0690X00000DXT5DQAX.png

JW

pbayton9
pbayton9Author
Associate II
February 27, 2020

Many thanks +++. It could still be better documented in the next revision of the manual please.