Skip to main content
antonioB
Associate III
February 26, 2020
Question

STM32F746GDISCOVERY and TouchGFX 4.13 problem

  • February 26, 2020
  • 2 replies
  • 820 views

Hi to all i have this problem, i create a simpe example with TouchGFX Designer 4.13, i use the STM32F746GDISCOVERY for my test.

I create the esample and i see all work well because i run simulator and run target all work well.

I generate the code, i open the project with CubeIde 1.3 and in folder ..Middlewares\ST\touchgfx copy the files present in TouchGFX folder,

If i build the project i don't have error this is the output:

11:11:51 **** Incremental Build of configuration Debug for project STM32F746G_DISCO ****

make -j8 all

arm-none-eabi-size STM32F746G_DISCO.elf

 text    data     bss     dec     hex  filename

 44976     192    9812   54980    d6c4  STM32F746G_DISCO.elf

Finished building: default.size.stdout

11:12:14 Build Finished. 0 errors, 0 warnings. (took 22s.711ms)

if i run the debug i have this error:

STMicroelectronics ST-LINK GDB server. Version 5.5.0

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

      Persistent Mode          : Disabled

      Logging Level            : 1

      Listen Port Number       : 61234

      Status Refresh Delay     : 15s

      Verbose Mode             : Disabled

      SWD Debug                : Enabled

      InitWhile                : Enabled

Waiting for debugger connection...

Debugger connected

    -------------------------------------------------------------------

                     STM32CubeProgrammer v2.4.0                

    -------------------------------------------------------------------

ST-LINK SN : 0676FF535651727067074056

ST-LINK FW : V2J36M26

Voltage   : 3.20V

SWD freq  : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID : 0x449

Device name : STM32F74x/STM32F75x

Flash size : 1 MBytes

Device type : MCU

Device CPU : Cortex-M7

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a20696.srec

 File        : ST-LINK_GDB_server_a20696.srec

 Size        : 44728 Bytes

 Address     : 0x08000000

Erasing memory corresponding to segment 0:

Erasing internal memory sectors [0 1]

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:02.196

Verifying ...

Download verified successfully

(Read)Failed determine breakpoint type

Error! Failed to read target status

Debugger connection lost.

Shutting down...

i don't know where is the problem

can you help me?

This topic has been closed for replies.

2 replies

mattias norlander
ST Employee
February 26, 2020

Do you have any breakpoints set in the QSPI flash memory at 0x90000000ish?

First try removing all breakpoint using the Breakpoints view.

Does that help?

If not, try to remove the debug configuration and create a new one with default settings. You may also disable the checkbox "set breakpint at main" and "Resume" on the startup tab of the debug config to see if you are able to step into the Reset_Handler without problems?!

Not working?

What if you try using OpenOCD instead instead of ST-LINK GDB server as the probe choice in the debug config?

antonioB
antonioBAuthor
Associate III
February 27, 2020

Hi, i clear all breakpoint, but don't fix it.

i use OpenCD and i have this message:

Open On-Chip Debugger 0.10.0+dev-01193-g5ce997d (2020-02-20-10:57)

Licensed under GNU GPL v2

For bug reports, read

   http://openocd.org/doc/doxygen/bugs.html

srst_only separate srst_nogate srst_open_drain connect_assert_srst

Info : The selected transport took over low-level target control. The results might differ compared to plain JTAG/SWD

adapter speed: 8000 kHz

adapter_nsrst_delay: 100

Info : Listening on port 6666 for tcl connections

Info : Listening on port 4444 for telnet connections

Info : clock speed 8000 kHz

Info : STLINK V2J36S26 (API v2) VID:PID 0483:374B

Info : using stlink api v2

Info : Target voltage: 3.204180

Info : SRST line asserted

Warn : Silicon bug: single stepping will enter pending exception handler!

Info : STM32F746NGHx.cpu: hardware has 8 breakpoints, 4 watchpoints

Info : Listening on port 3333 for gdb connections

Info : accepting 'gdb' connection on tcp/3333

Info : SRST line released

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0xb9337822 msp: 0x4c05b510

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

adapter speed: 4000 kHz

Info : device id = 0x10016449

Info : flash size = 1024kbytes

Info : SRST line asserted

Info : SRST line released

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0xb9337822 msp: 0x4c05b510

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

Info : Unable to match requested speed 8000 kHz, using 4000 kHz

adapter speed: 4000 kHz

target halted due to breakpoint, current mode: Thread

xPSR: 0x61000000 pc: 0x20000044 msp: 0x4c05b510

Info : SRST line asserted

Info : SRST line released

target halted due to debug-request, current mode: Thread

xPSR: 0x01000000 pc: 0xb9337822 msp: 0x4c05b510

and this immage

0690X00000DXSo7QAH.png

you can see that i don't run the resume, if I comment the scheduler

// osKernelStart();

I always have the same problem, don't run the program