Skip to main content
JWu.3
Associate
February 25, 2020
Question

SensorTile Datalog to SD cannot reach 500 Hz?

  • February 25, 2020
  • 1 reply
  • 674 views

I am using STSW-STLKT01_V2.1.1 package Datalog project to program the sensortile. It works perfectly at 200Hz logging acc+ gyro+ Magnetometer data. I disabled all other sensors. However, if I increase the logging frequency to 500 Hz, it work for 5 seconds and shut down automatically. Does anybody know why?

    This topic has been closed for replies.

    1 reply

    Eleon BORLINI
    ST Employee
    February 25, 2020

    Hi @JWu.3​ , please consider that a new FW version (2.2.0) is available, you can try with this revision if the issue is solved. Btw, please note that the STSW-STLKT01 package is not optimized to manage higher rates than default, differently from newer platforms such as the STWINKT1, whose data-logging and data management in general is optimized for every ODR. Regards