Question
Feature Request: HAL_UART_DMAPauseReceive, HAL_UART_DMAPauseTransmit
Currently the STM32_L4 HAL provides HAL_UART_DMAPause and HAL_UART_DMAResume. These pause/resume both TX and RX on the UART.
I am using DMA for both transmit and receive on a UART. I have a case where I need to pause the receive (for flow control) but must still continue to transmit. It would be desirable to have this feature available in the HAL. For now I have resorted to copying the HAL_UART_DMAPause & HAL_UART_DMAResume code and removing the TX bits to make it work for my needs.