Skip to main content
Tss.1
Associate
February 23, 2020
Question

How can i solve the Data transmission error problem in STM32 Lora and Sigfox Discovery kit for STM32F072 MCU to sigfox network interface?

  • February 23, 2020
  • 3 replies
  • 2416 views

I had purchased two STM32 Lora and Sigfox Discovery kit for STM32F072 MCU.

I am using this for sigfox data transmitting purpose for our prototype designing . I had uploaded the AT commands code on both dev.boards, One board is completely working and the data can be sent to sigfox network interface (using the command "AT$SF=1010" or "AT$SB=1") followed by an OK response.

but the another dev.board is not transmitting the data and didn't get an OK response. (All the hardware configurations are same on both dev.boards).

Sir, please help for troubleshooting this issue as soon as possible.

This topic has been closed for replies.

3 replies

Uwe Bonnes
Chief
February 23, 2020

Sigfox and Lorawan have a lot of specific numbers which need registration with the network provider. Did you register both devices with the right identification numbers?

Tss.1
Tss.1Author
Associate
February 23, 2020

We are using a Sigfox SDR Dongle for our testing purpose .

Both the device id are being saved at the  sigfox network interface.

Tss.1
Tss.1Author
Associate
February 23, 2020

..