CR95HF transceiver antenna tuning - conflicting information/measurements regarding voltage on ST_R0 and RX1 resp. RX2 Pin
- 1 reply
- 1579 views
Hi there,
I made a design with the CR95HF and it's working. The design of the EMI filter and matching circuit is done like on the X-NUCLEO-NFC03A1 NFC card reader board, see [UM1799] page 12.
I'd now like to tune the components on my design to increase the reader performance. In [AN4327] on page 15, there is a point saying: "Measure the DC voltage in the ST_R0 pin: adjust the ZRX component value to limit the voltage measured on ST_R0 below 7 V." I guess it's to make sure, the differential voltage between RX1 and RX2 stays within the allowed range, because if it is above 7 V one should adjust ZRX.
If I'm measuring the voltage between GND and ST_R0, I measure an average value of 8.6 V in my design (see hhd-gnd_str0.png). On the X-NUCLEO-NFC03A1, I measure 9.8 V (see nucleo-gnd_str0.png). Both voltages are over the recommended 7 V from [AN4327].
However if I'm measuring the voltage between pin RX1 and RX2, I'm far away from the maximum differential voltage of 18 V mentioned in [CR95HF] page 47 (see hhd-rx1_rx2.png and nucleo-rx1_rx2.png).
My questions:
What does the voltage on pin ST_R0 indicate?
Is it no problem to have a voltage above 7 V @ ST_R0 pin?
If it is no problem, why is it mentioned the way it is in [AN4327]?
If it is a problem, why is it around 10 V on the X-NUCLEO-NFC03A1 NFC card reader board?
Best regards
teysachaux
===
[UM1799] Getting started with X-NUCLEO-NFC03A1 NFC card reader board based on CR95HF for STM32 Nucleo - https://www.st.com/content/ccc/resource/technical/document/user_manual/6b/a3/ef/49/6b/75/43/04/DM00125142.pdf/files/DM00125142.pdf/jcr:content/translations/en.DM00125142.pdf
[AN4327] CR95HF tuning circuit with an EMI filter - https://www.st.com/content/ccc/resource/technical/document/application_note/8e/99/77/a7/4f/58/4d/d6/DM00089926.pdf/files/DM00089926.pdf/jcr:content/translations/en.DM00089926.pdf
[CR95HF] 13.56-MHz multi-protocol contactless transceiver IC with SPI and UART serial access - https://www.st.com/resource/en/datasheet/cr95hf.pdf