Skip to main content
RZ_it
Associate II
February 21, 2020
Question

What is the function of PA13 (BOOTFAILN) on the STM32MP15x

  • February 21, 2020
  • 1 reply
  • 1110 views

I'm working on a design with the STM32MP153 and came across the additional function of PA13 as BOOTFAILN.

I can guess what this means but I can't find any documentation on the subject. Don't know when or why this pin gets active. Or is it an input? In the reference design schematics both a LED and a switch are connected to this pin.

Thanks for any insight.

This topic has been closed for replies.

1 reply

PatrickF
ST Employee
February 21, 2020

please have a look to https://wiki.st.com/stm32mpu/wiki/STM32MP15_ROM_code_overview#Debug_and_Error_messages and also 8.3.5 "Debug triggers and LEDs" of AN5031

In order to give better visibility on the answered topics, please click on 'Best Answer' on the reply which solved your issue or answered your question.Tip of the day: Try Sidekick STM32 AI agent