What is the time it takes for the STM32l082kb to wake up it's adc? and is a ferrite bead necessary?
For my new project i have to use an ADC to measure the peak value of a pulse. This pulse wakes up the microcontroller from stop mode, and the processor has to wake up the internal adc to take the samples needed. Unfortunately i can't find the time it takes for the adc to wake up in the datasheets, if the wake up time is too high i might have to consider getting an external one. Furthermore, in the hardware reference for my microcontroller there is a ferrite bead included to stabilize and filter the adc input voltage, if i use the adc it will be with a Vref of 3,3Volts and i will use the 12-bit adc to measure in steps of preferrably 10mV. I have read online that a ferrite bead is recommended and can make a big difference, but i can't find how to select the proper one.