Skip to main content
LScho.1
Visitor II
February 21, 2020
Question

IIS2DH datasheet : soldering information unclear

  • February 21, 2020
  • 1 reply
  • 592 views

in the datasheet in section 3.1, it is mentioned to leave "pin 1 indicator" unconnected during soldering. Can this be clarified? Pin 1 is a functional pin and is always connected for a clock signal. How can we use this device if it is not allowed to connect the pin when soldering?

This topic has been closed for replies.

1 reply

Eleon BORLINI
ST Employee
February 21, 2020

Hi @LScho.1​ , i believe it is a refuse from other part numbers that have a "Pin1 indicator" such as the one below:

0690X00000DC4jGQAT.png

Please don't care of that instruction. Btw of course don't power up the device during soldering phase! Regards