Skip to main content
NWeis.19
Associate II
February 19, 2020
Question

Hi, I am working on a new project with the STM32WB, I need a server with two connection. The example p2pServer code has just one connection. Is there another example or more literature on the subject ? Thanks.

  • February 19, 2020
  • 0 replies
  • 454 views

My project consists of two STM32WB A master and a slave. The master will run the p2pRrouter example with some modifications and the slave will run the p2pServer preferably with two connections.

both Master and slave needs to communicate with each other and with an external app

This topic has been closed for replies.