Cant generate code, because CubeIDE didn't find firmware in /STM32Cube/Repository/ which was automatically downloaded installed
Fresh installation, when I try to create a STM32 project a zip file with firmware is downloaded and unpacked, but I still get this error message:
"Code generation could not be done because necessary firmware package is missing. Not able to complete STM32Cube project."
I tried to download and unzip these files manually with no luck.
I have this issue on my both PCs with windows 10. Also the same thing happens regardless if I try to create a project for my Nucleo F030R8 or Nucleo L053R8.