Skip to main content
Jace
Associate II
February 14, 2020
Solved

Can I use the TrueStudio for the P-NUCLEO-IHM001 board?

  • February 14, 2020
  • 15 replies
  • 3427 views

..

This topic has been closed for replies.
Best answer by BTrem.1

I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.

15 replies

berendi
Principal
February 14, 2020

Yes. It has a STM32F302R8 MCU, any development environment can be used that supports it (or Cortex-M4 in general).

Ozone
Principal
February 14, 2020

With the buy up of Atollic by ST, TrueStudio is more or less obsolete. I would not expect extensive support from ST.

Claire O.
ST Employee
February 14, 2020

Dear SPark.2,

I can confirm than the MCSDK is still ok with TrueStudio for yout board.

Thanks and best regards,

Claire

Jace
JaceAuthor
Associate II
February 17, 2020

Thank you for all your answers.

Jace
JaceAuthor
Associate II
February 17, 2020

Hi,

I bought a P-NUCLEO-IHM001 board and tried to generate c code as follow.

  1. Copied the "PotentiometerAdvance" folder to another location.
  2. Run the ST Motor Control Workbench (V5.4.3) and opened project "PotentiometerAdvance.stmcx"
  3. Project Generation
  4. Click "GENERATE" button
  5. RUN STM32Cube
  6. Selected TrueSTUDIO at Toolchain /IDE​ box
  7. GENERATE CODE and Opened project with Atollic TrueSTUDE IDE
  8. Selected "Build All" but I found next error

" fatal error: stm32f3xx_ll_bus.h: No such file or directory "

How can I fix it? Please guide me.

Thanks

Jace
JaceAuthor
Associate II
February 17, 2020

I solved the error but errors are continue..more and more.

Too many errors are generated. so I'll give up to use TrueSTUDIO.

BTrem.1
Senior
March 4, 2020

I have the same hardware and went through the same steps described in the Project Potentiometer readme.txt file. I don't think its a TrueStudio Problem.

  1. Run ST MC Workbench 5.4.3
  2. Open potentiometer.stmcx and save to a new location.
  3. Select Generate--> build with ST32CubeIDE Tool chain (Update not given as option)
  4. Run ST32CubeMX and Generate Code
  5. Open project with IDE from STM32CubeMX.ioc file
  6. FW_F3 V1.11.0 is not latest, choose to migrate project
  7. Build All resulted in 9 errors, such as: fatal error: stm32f3xx_ll_bus.h: No such file or directory

I am trying to get local ST FAE help on this, very frustrated for 3 weeks now.

Claire O.
ST Employee
March 5, 2020

Dear Jace and BTrem.1,

Can you please check which version of CubeIDE or TrueStudio you are using?

We will check your problems,

Claire

BTrem.1
Senior
March 5, 2020

I'm using SDK 5.4.3. I believe this is the latest available to date.

Claire O.
ST Employee
March 5, 2020

That's the right version of MCSDK, Thanks!

Can you please check your IDE version as well?

BTrem.1
BTrem.1Best answer
Senior
March 5, 2020

I have been able to build and run projects in the SDK_5.4.3 directory using the Keil Tool chain (MDK-ARM) though on some I needed to optimize size not time, to keep below the 32k limit on the Lite version.

Laurent Ca...
Senior III
October 16, 2020

Dear @Jace​ , dear @BTrem.1​ 

Do you have still this problem to solve?

And just in case, if not, do not hesitate to share the final solution you found.

Best regards

Laurent Ca...

BTrem.1
Senior
October 16, 2020
Hi,
I ended up using Keil uVision 5.30, MDK-Arm Essential version. Sometimes I also use STM32CubeIDE.
Brian