Skip to main content
JYang.4
Associate
February 13, 2020
Solved

STM32F4-Not seeing an I2C signal

  • February 13, 2020
  • 1 reply
  • 655 views

Hi,

I'm using an STM32F429 MCU and trying to connect to a sensor through I2C. However, I measured both I2C pins with an oscilloscope and they were not showing any clock pulse or a signal. Here's my code for initiation:

void MX_I2C1_Init(void)
{
 hi2c1.Instance = I2C1;
 hi2c1.Init.ClockSpeed = 100000;
 hi2c1.Init.DutyCycle = I2C_DUTYCYCLE_2;
 hi2c1.Init.OwnAddress1 = 0;
 hi2c1.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
 hi2c1.Init.DualAddressMode = I2C_DUALADDRESS_DISABLE;
 hi2c1.Init.OwnAddress2 = 0;
 hi2c1.Init.GeneralCallMode = I2C_GENERALCALL_DISABLE;
 hi2c1.Init.NoStretchMode = I2C_NOSTRETCH_DISABLE;
 if (HAL_I2C_Init(&hi2c1) != HAL_OK)
 {
 Error_Handler();
 printf("I2C Initiation Failed!\r\n");
 }
}
 
void HAL_I2C_MspInit(I2C_HandleTypeDef* i2cHandle)
{
 
 GPIO_InitTypeDef GPIO_InitStruct;
 if(i2cHandle->Instance==I2C1)
 {
 __GPIOB_CLK_ENABLE();
 /* I2C1 clock enable */
 __I2C1_CLK_ENABLE();
 /**I2C1 GPIO Configuration 
 PB8 ------> I2C1_SCL
 PB9 ------> I2C1_SDA 
 */
 GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_9;
 GPIO_InitStruct.Mode = GPIO_MODE_AF_OD;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
 GPIO_InitStruct.Alternate = GPIO_AF4_I2C1;
 HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
 }
}

And the following code for testing:

 while (1)
 {
 unsigned char buf;
 HAL_I2C_Mem_Read(&hi2c1, 0x29, 4, I2C_MEMADD_SIZE_8BIT, buf, 1, 10000);
 printf("Testing!\r\n");
 HAL_Delay(1000);
 }

I believe I measured the correct pins(PB8 and PB9), but I was not even seeing an SCL signal. The slave device was not connected yet. Does it have to be connected to see a clock signal? Or is there anything wrong with the code? Thanks.

This topic has been closed for replies.
Best answer by JYang.4

Problem solved after connecting the sensor to the MCU.

1 reply

JYang.4
JYang.4AuthorBest answer
Associate
February 13, 2020

Problem solved after connecting the sensor to the MCU.