Skip to main content
Mdi c
Associate III
February 11, 2020
Question

ADC scan continuous mode with DMA in STM32H7 - all values are 0.

  • February 11, 2020
  • 8 replies
  • 4774 views

Dear all,

I am trying to read 3 ADCs channels using scan continuous mode and DMA with a STM32H7 (ADC3). Below the CubeMx settings + DMA.

0690X00000D9TejQAF.png0690X00000D9TfXQAV.png

In the main, before the While(1) loop I start the ADC with:

HAL_ADC_Start_DMA(&hadc3, (uint32_t*)adc_data, 3) ;

Where ADC_Values is uint32_t adc_data[3];

When I run the debugger, adc_data is always 0x0000.

Any hint?

Thanks

This topic has been closed for replies.

8 replies

Yoichi Shinoda
Senior
February 12, 2020

Are you handling the buffer coherency issue for ADC DMA read buffer correctly?

https://community.st.com/s/article/FAQ-DMA-is-not-working-on-STM32H7-devices

Mdi c
Mdi cAuthor
Associate III
February 12, 2020

Hello @Yoichi Shinoda​ , thank you for your answer. I came accross that article and I think that's the issue I have. I tried to follow it but I think my knowledge about STM32 MCUs is too limited to really understand it ..

Imen GH
ST Employee
February 27, 2020

Hello,

You should change the memory address, as shown in Figure (when using IAR)

 Please find attached the RM0433 Rev 6  (page 101, 128) link for more clarification

Regards

0690X00000DXQe5QAH.png

Nesrine.JLASSI
Visitor II
March 10, 2020

Hi all,

User have to do this update

define symbol __ICFEDIT_region_RAM_start__ = 0x24000000;

define symbol __ICFEDIT_region_RAM_end__ = 0x2407FFFF;

manually (in the stm32h743xx_flash.icf ) since linker file is not managed by STM32CubeMX (copied from the FW package).

Best regards,

Nesrine

Mdi c
Mdi cAuthor
Associate III
April 3, 2020

Dear @Nesrine.JLASSI​ , is this equivalent to setting the IRAM2 region in the target option in Keil ?

0693W000000VGhrQAG.jpg

Mdi c
Mdi cAuthor
Associate III
April 3, 2020

Hello @Nesrine.JLASSI​  and @Imen GH​ , modifying the IRAM2 in Keil did the trick. Now I can see the data being acquired by the MCU. However, I noticed that despite the ADC resolution is set to 16bits, I can only read 8bits since the the 8 LSBs are always 0, as shown in the debugger view below:

0693W000000VIdXQAW.jpg

where :

uint16_t adc_data[7];

HAL_ADC_Start_DMA(&hadc1, (uint32_t*)adc_data, 7) ;

ADC initialization code:

static void MX_ADC1_Init(void)

{

 /* USER CODE BEGIN ADC1_Init 0 */

 /* USER CODE END ADC1_Init 0 */

 ADC_MultiModeTypeDef multimode = {0};

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC1_Init 1 */

 /* USER CODE END ADC1_Init 1 */

 /** Common config 

 */

 hadc1.Instance = ADC1;

 hadc1.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1;

 hadc1.Init.Resolution = ADC_RESOLUTION_16B;

 hadc1.Init.ScanConvMode = ADC_SCAN_ENABLE;

 hadc1.Init.EOCSelection = ADC_EOC_SEQ_CONV;

 hadc1.Init.LowPowerAutoWait = DISABLE;

 hadc1.Init.ContinuousConvMode = ENABLE;

 hadc1.Init.NbrOfConversion = 7;

 hadc1.Init.DiscontinuousConvMode = DISABLE;

 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;

 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 hadc1.Init.ConversionDataManagement = ADC_CONVERSIONDATA_DMA_CIRCULAR;

 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;

 hadc1.Init.LeftBitShift = ADC_LEFTBITSHIFT_NONE;

 hadc1.Init.OversamplingMode = ENABLE;

 hadc1.Init.Oversampling.Ratio = 8;

 hadc1.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_3;

 hadc1.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;

 hadc1.Init.Oversampling.OversamplingStopReset = ADC_REGOVERSAMPLING_CONTINUED_MODE;

 if (HAL_ADC_Init(&hadc1) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure the ADC multi-mode 

 */

 multimode.Mode = ADC_MODE_INDEPENDENT;

 if (HAL_ADCEx_MultiModeConfigChannel(&hadc1, &multimode) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_3;

 sConfig.Rank = ADC_REGULAR_RANK_1;

 sConfig.SamplingTime = ADC_SAMPLETIME_387CYCLES_5;

 sConfig.SingleDiff = ADC_SINGLE_ENDED;

 sConfig.OffsetNumber = ADC_OFFSET_NONE;

 sConfig.Offset = 0;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_4;

 sConfig.Rank = ADC_REGULAR_RANK_2;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_5;

 sConfig.Rank = ADC_REGULAR_RANK_3;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_9;

 sConfig.Rank = ADC_REGULAR_RANK_4;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_14;

 sConfig.Rank = ADC_REGULAR_RANK_5;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_15;

 sConfig.Rank = ADC_REGULAR_RANK_6;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /** Configure Regular Channel 

 */

 sConfig.Channel = ADC_CHANNEL_19;

 sConfig.Rank = ADC_REGULAR_RANK_7;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)

 {

  Error_Handler();

 }

 /* USER CODE BEGIN ADC1_Init 2 */

 /* USER CODE END ADC1_Init 2 */

}